Skip to main content
Visitor II
Aug 18, 2025 6:33 AM UTC
Solved

Does IHM09M2 can connect with NUCLEO-H755ZI-Q

Can X-NUCLEO-IHM09M2 (adapter board) connect with NUCLEO-H755ZI-Q (controller board) using male and female connector(without flying wire)? 

This topic has been closed for replies.
GMA
GMABest answer
ST Technical Moderator
Aug 18, 2025 2:27 PM UTC

Hello @Maverick,

You must verify that all the required signals are available. If they are not available, add the necessary wires and update the X-NUCLEO-IHM09M2.json file located in the MC_SDK_x.x.x\Utilities\PC_Software\STMCWB\assets\hardware\board\adapter directory.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

1 reply

GMA
GMABest answer
ST Technical Moderator
Aug 18, 2025 2:27 PM UTC

Hello @Maverick,

You must verify that all the required signals are available. If they are not available, add the necessary wires and update the X-NUCLEO-IHM09M2.json file located in the MC_SDK_x.x.x\Utilities\PC_Software\STMCWB\assets\hardware\board\adapter directory.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA