Skip to main content
JEsca.1
Associate II
Apr 1, 2020 8:11 PM UTC
Question

Difference in ST Motor Control Workbench between Sensor displacement and placement electrical angle

Dear,

It not clear for me, here :

In my case Hall sensor are physically spaced by 60 deg, I am not sure how to setup these 2 parameters.

Any help appreciated.

Regards

This topic has been closed for replies.

3 replies

Enrico Poli
ST Employee
Apr 7, 2020 8:00 AM UTC

The displacement is the Hall spacing, and the electrical angle is the equivalent electrical position of the Hall sensor H1 rising edge.

The zero of the electrical angle is the peak of phase A BEMF (OUT1). In your case, I think should be zero, but you should check the motor datasheet.

Enrico

CLutz.1
Visitor II
Apr 21, 2020 9:09 AM UTC

in other words:

sensor displacement typical is 60° or 120° and it is same between H1 to H2 and H2 to H3.

placement electrical angle is like offset of hall sensor arrangement to motor stator.

Laurent Ca...
Senior III
Jun 22, 2021 5:36 AM UTC

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards