Skip to main content
DMeie.2
Associate III
October 4, 2024
Question

Difference between NOMINAL_CURRENT and IQMAX

I need to implement runtime current limitation.

Another thread says to use "PID_SetUpperOutputLimit" on the PidSpeedHandle for that to change the values originally defined by IQMAX, which makes sense.
However, I also found NOMINAL_CURRENT used for MaxPositiveTorque and MinNegativeTorque in SpeednTorqCtrl, which has been set by the MCWB tool to the same value as IQMAX.

What are these values used for? Do I have to change them as well? There doesn't seem to be a function for that.
NOMINAL_CURRENT is not mentioned in the SDK documentation and a comment in pmsm_motor_parameters.h only says it is used when  Id = 0 "to saturate the output of the PID for speed regulation" (so it does the same than changing IQMAX?), even though there's no Id to set anywhere.

This topic has been closed for replies.