Skip to main content
This topic has been closed for replies.
Fred V.
Fred V.Best answer
ST Employee
June 27, 2022

Hello,

Enabled stands for FOC (Field Oriented Control). The name is confusing and should be changed. It dates back from the time when the only supported drive technique was FOC. When Enabled is active, the Motor Control Middleware is configured to drive a PMSM motor with the FOC technique.

The SixStep mode is active when the Motor Control Middleware is configured to drive a motor using the Six Step technique

The Induction mode is active when the Motor Control Middleware is configured to drive an asynchronous motor.

Only one of these modes can be active at any time. The active mode must not be changed from within STM32CubeMx as it would result in the generation of a not working project.

To configure the Motor Control Middleware, use the Motor Control Workbench delivered with ST Motor Control SDK (X-CUBE-MCSDK).

I hope it'll help.

Best regards

Fred

5 replies

Fred V.
Fred V.Best answer
ST Employee
June 27, 2022

Hello,

Enabled stands for FOC (Field Oriented Control). The name is confusing and should be changed. It dates back from the time when the only supported drive technique was FOC. When Enabled is active, the Motor Control Middleware is configured to drive a PMSM motor with the FOC technique.

The SixStep mode is active when the Motor Control Middleware is configured to drive a motor using the Six Step technique

The Induction mode is active when the Motor Control Middleware is configured to drive an asynchronous motor.

Only one of these modes can be active at any time. The active mode must not be changed from within STM32CubeMx as it would result in the generation of a not working project.

To configure the Motor Control Middleware, use the Motor Control Workbench delivered with ST Motor Control SDK (X-CUBE-MCSDK).

I hope it'll help.

Best regards

Fred

Dane._.T
Dane._.TAuthor
Associate II
June 27, 2022

Thanks for the explanation!

Unfortunately, I cannot get MCSDK to generate the Middleware with the Induction option, as it either does not appear (v. 6.0.0) or it fails to generate pwm_curr_fdbk.c properly (v. 5.Y.4). The other two generate fine and can run my setups. From what I've seen so far, Induction seems to be newer and is only supported in 5.Y.x.

Dane._.T
Dane._.TAuthor
Associate II
June 27, 2022

[mistake]

Fred V.
ST Employee
June 27, 2022

You're welcome.

Indeed, Induction motors are not fully supported yet. In MCSDK 5.Y.*, they are only supported through one example that works one hardware configuration. On MCSDK 6, the support for these motors has not been reintroduced yet. It ill be, but I cannot tell when.

The ACIM example is broken on MCSDK 5.Y.4. But, it should work with MCSDK 5.Y.3, the previous version which is still available (under the label 5.5.3 on ST.com).

I hope this will help you.