Current sensing in 6-step mode with EVLSPIN32G0A2
Hi guys,
I'm using Motor Control Workbench (V6.4.2) with the EVLSPIN32G0A2 in a 6-step configuration with Hall sensors.
At the moment, it seems that the motor current cannot be measured and monitored in Motor Pilot.
Is there any option to activate current sensing for this board in 6-step mode, or do I need to implement the current measurement myself?
The hardware itself should support current sensing, since current measurement is also available when using the same board in an FOC configuration.
Is there an easy workaround to get the motor current?
Thanks!