Skip to main content
Associate II
August 15, 2025
Question

Controlling an ESC002V1 board through a UART connection

  • August 15, 2025
  • 3 replies
  • 468 views

I'm trying to control a BLDC motor attached to a STEVAL-ESC002V1 board though the UART connection, but so far without success.

I updated the symbols and recompiled the supplied firmware to disable the PWM control and enable the UART. It compiled without errors and I was able to upload the BIN file to the board.

Then using a terminal app on my laptop, I connected it using a USB-UART interface, to connector J2 on the board. The settings were 57600,8,1,Even, Noflow control.

However after rebooting the board I was unable to get any output on the terminal, nor sending any commands to the board.

Am I missing something ?

 

 

This topic has been closed for replies.

3 replies

GMA
ST Technical Moderator
August 19, 2025

Hello @pjrebordao,

Is the default provided firmware functional?
Did you review previous STEVAL-ESC002V1 posts, such as this one?

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Associate II
August 19, 2025

I didn't use the firmware exactly as provided because I really need the control via UART.

So I changed the required symbols and recompiled the source on the IAR workbench.

The compilation gave no errors and I was able to successfuly upload the code using the STM32Programmer with the bootload connector.

Associate II
August 23, 2025

Any ideas regarding this issue ?