Skip to main content
Duc
Senior
Jul 21, 2025 2:45 PM UTC
Solved

Compatibility of Nucleo-H755ZI with X-NUCLEO-IHM07M1

Hello STM community,

I am planning to use the Nucleo-H755ZI board (STM32H7 series) in combination with the X-NUCLEO-IHM07M1 motor driver expansion board, and I have a couple of questions regarding compatibility and setup:

  1. Compatibility:

    • Is the Nucleo-H755ZI board fully compatible with the X-NUCLEO-IHM07M1 motor driver expansion when plugged directly into the Arduino-compatible headers (MORPHO header)? I want to ensure that the board can drive motors as intended without any issues in terms of voltage levels or pin mappings.

  2. Required Modifications:

    • Does the Nucleo-H755ZI-Q variant (specifically) require any modifications or special considerations for proper integration with the X-NUCLEO-IHM07M1? I am aware that the STM32 Nucleo boards generally follow the same Arduino pinout, but I want to confirm if there are any specific steps or precautions I should take when using this combination.

Any help or insights from someone who has already worked with this combination would be much appreciated!

Thank you!

This topic has been closed for replies.
GMA
GMABest answer
ST Technical Moderator
Jul 21, 2025 4:21 PM UTC

Hello @Duc,

Using MCSDK 6.4.0 Workbench and generating a Nucleo-H755ZI/X-NUCLEO-IHM07M1 project, you will be able to know if configuration is supported or not.
Once project generated, refer to "FOC Wizard" GUI, "Pins Usage & Hw" Tab, "Hardware Changes" part lists all required hardware modifications to be considered.

GMA_1-1753114672879.png

 

 

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

3 replies

GMA
GMABest answer
ST Technical Moderator
Jul 21, 2025 4:21 PM UTC

Hello @Duc,

Using MCSDK 6.4.0 Workbench and generating a Nucleo-H755ZI/X-NUCLEO-IHM07M1 project, you will be able to know if configuration is supported or not.
Once project generated, refer to "FOC Wizard" GUI, "Pins Usage & Hw" Tab, "Hardware Changes" part lists all required hardware modifications to be considered.

GMA_1-1753114672879.png

 

 

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Duc
DucAuthor
Senior
Jul 22, 2025 3:05 PM UTC

Hi @GMA,

Thank you for your helpful response regarding the need to remove SB80 (RMII_REF_CLK) and SB84 (RMII_MDC) when using the Nucleo-H755ZI-Q with the X-NUCLEO-IHM07M1 motor driver expansion board.

I have a few follow-up questions:

  1. What is the specific impact of removing SB80 and SB84 on the rest of the board’s functionality?
    I understand these are related to RMII (Ethernet), but does removing them affect anything else beyond the Ethernet function?

  2. Is it necessary to remove and re-solder these SBs every time I switch between motor control and Ethernet functionality?
    For example, if I want to use both motor control (IHM07M1) and Ethernet at different times, will I have to constantly solder/desolder SB80 and SB84?

Any advice or experience you can share would be much appreciated!

Best regards,

Duc Le

GMA
ST Technical Moderator
Jul 22, 2025 3:37 PM UTC

Hello @Duc,

1. For Motor Control use case, there is no impact.
2. You can order a second board for Ethernet use case.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA