Skip to main content
ADiab.2
Visitor II
September 16, 2021
Question

Can you help me for (Are there videos for the starting guide for the STM3210B-MCKIT PMSM starter control kit?

I have STM3210B-MCKIT PMSM starter control kit, It is worked through LCD and for start and stop the motor.

but I would like to develop a new controller and change the control system. I would like to a guide and If there is a library that has the projects for this starter kit?

how can I measure the currents with an oscilloscope through ADC, I can find these pins in the kit?

I asked after a spent a long time, so please help me!

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
October 20, 2021

Dear @ADiab.2​ 

Welcome to the STM32 Community

Sorry for late answer.

Could you give more details to the STM32 Community about your setup -the material you use- ?

(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)

And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?

Best regards