Question
Can the resolution of the motor speed measurement code be increased?
I have an application where I am running a light inertia motor (6 pole-pair) at a constant speed of nominally 1800 rpm. In this application I need finer control than is provided by the speed measurement resolution. I am already using SPEED_UNIT _001Hz.
Is there any means to modify the code so that I can improve the resolution by a factor of 4 or 5? I am going through the Motor Control files and trying to figure out where I might make the necessary modifications.