Skip to main content
LTren.1
Visitor II
July 12, 2021
Question

Can STEVAL-SPIN3201 be programmed for sensorless 6step? I try to use X-CUBE-MCSDK-Y (6S_STEVAL3201_SL_VM) but when i use the Keil and download it to the board, the motor don't work and i can't connect to the motor pilot 5.Y.1

Hi ST Community,

I'm seeking to start a motor with FOC and six-steps to analyze the difference. When i used the FOC example it works fine, but when i change something and download it to the board with Keil the motor control workbench don't connect: Connection failed! No response, check the communication cable...

At least the example BullRunning works, but the 6steps (6S_STEVAL3201_SL_VM) do nothing

What I'm doing wrong?

what i can do to change configurations on the BullRunning and still connect the board to the motor control workbench?

To use 6steps, i need to change something on the board?

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
July 14, 2021

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards