Skip to main content
PKris
Associate
Sep 7, 2018 7:12 AM UTC
Solved

Can MCSDK be used for driving 3-Phase ACIM?

MCSDK has options only for PMSM. I would like to know whether MCSDK can also be used to control 3-Phase ACIM. If so, any details on the changes required will be helpful.

Thanks,

Prakash

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:38 PM UTC

Dear @PKris​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

4 replies

Claire O.
ST Employee
Sep 7, 2018 2:46 PM UTC

Dear Prakash,

Sorry but 3-Phase ACIM has not yet been implemented.

Thanks and best regards,

Claire

Laurent Ca...
Senior III
Jun 28, 2021 5:27 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:38 PM UTC

Dear @PKris​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

PKris
PKrisAuthor
Associate
Jun 28, 2021 1:38 PM UTC

Hi @Laurent Ca...​ 

Thanks for the information. I'll definitely take a look at it.