I have been able to build and run projects in the SDK_5.4.3 directory using the Keil Tool chain (MDK-ARM) though on some I needed to optimize size not time, to keep below the 32k limit on the Lite version.
I have the same hardware and went through the same steps described in the Project Potentiometer readme.txt file. I don't think its a TrueStudio Problem.
Run ST MC Workbench 5.4.3
Open potentiometer.stmcx and save to a new location.
Select Generate--> build with ST32CubeIDE Tool chain (Update not given as option)
Run ST32CubeMX and Generate Code
Open project with IDE from STM32CubeMX.ioc file
FW_F3 V1.11.0 is not latest, choose to migrate project
Build All resulted in 9 errors, such as: fatal error: stm32f3xx_ll_bus.h: No such file or directory
I am trying to get local ST FAE help on this, very frustrated for 3 weeks now.
I have been able to build and run projects in the SDK_5.4.3 directory using the Keil Tool chain (MDK-ARM) though on some I needed to optimize size not time, to keep below the 32k limit on the Lite version.