Skip to main content
JLee.56
Visitor II
Jul 20, 2021 5:19 AM UTC
Solved

Can I use STSPIN32G4 with X-CUBE-MCSDK for ultra-high speed PMSM?

Hi, I am studying for ultra-high speed PMSM (about 100krpm, 700~1000W).

​

The motor is 2pole/3slots/3-phases sensorless motor.

I think STSPIN32G4 is a suitable driver for my motor in the electrical specification.

​

Just I want to check that I can freely control the motor using the driver with X-CUBE-MCSDK (I mean torque and speed controls).

Thank you.

This topic has been closed for replies.
Cristiana SCARAMEL
ST Employee
Aug 4, 2021 11:02 AM UTC

Hi @JLee.56​,

I confirm that the STSPIN32G4 is able to drive a motor (single pole pairs) in the above mentioned conditions (sensorless, ultra-high speed).

As already stated by @Laurent Ca...​ it is possible to perform torque and speed controls with the X-CUBE-MCSDK (in the Rev Y you can find a firmware example for the EVSPIN32G4 evaluation board).

Let me know if I solved your doubts, if so please "Select as Best" button.

"If you feel a post has answered your question, please click ""Accept as Solution"""

2 replies

Laurent Ca...
Senior III
Aug 3, 2021 4:59 AM UTC

Dear @JLee.56​ 

Yes you can control speed and torque with STM32 MC-SDK.

Regarding the possibility to do that at high speed, I just asked to our experts.

Best regards

Cristiana SCARAMEL
ST Employee
Aug 4, 2021 11:02 AM UTC

Hi @JLee.56​,

I confirm that the STSPIN32G4 is able to drive a motor (single pole pairs) in the above mentioned conditions (sensorless, ultra-high speed).

As already stated by @Laurent Ca...​ it is possible to perform torque and speed controls with the X-CUBE-MCSDK (in the Rev Y you can find a firmware example for the EVSPIN32G4 evaluation board).

Let me know if I solved your doubts, if so please "Select as Best" button.

"If you feel a post has answered your question, please click ""Accept as Solution"""