Skip to main content
TKara.2
Associate III
Dec 21, 2024 6:53 PM UTC
Solved

Can i use motor pilot with custom board

I can use a motor profiler with a custom board, but can I use a motor pilot with the same software? Is it possible to use a motor pilot with a custom board?

 
 
Gael A
Gael ABest answer
ST Employee
Jan 6, 2025 8:52 AM UTC

Hello TKara.2,

Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

4 replies

Gael A
Gael ABest answer
ST Employee
Jan 6, 2025 8:52 AM UTC

Hello TKara.2,

Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.
TKara.2
TKara.2Author
Associate III
Jan 7, 2025 2:40 AM UTC

Thanks @Gael A