Skip to main content
THA.1
Associate III
January 19, 2022
Question

(Bug Report) When using encoder, the generated code has a few defects - speed calculation is not reliable, no speed reliability check, and no scheme to clear speed feedback fault

(Environment)

MC_SDK 5.Y.3 + STM32CubeMX 6.3.0 with HAL + IAR EWARM 8.5

(Hardware)

custom board based on F446RE + custom power board + Low Voltage BLDC motor with Encoder

(Control Mode)

Speed Control

​

(What I found)

(1) speed calculation is not reliable

[ ENC_CalcAvrgMecSpeedUnit() in encoder_speed_pos_fdbk.c ]

Encoder direction and UP(overflow/underflow) count are used to calculate the delta.

This algorithm lead, however, to an incorrect result in the following case:

  • During speed loop (1msec), assume encoder direction has been up-counting so far
  • That is, speed is (+) and delta is (+)
  • However, just when ENC_CalcAvrgMecSpeedUnit() is called, encoder direction could be changed to down-counting
  • (+)delta and down-counting results in incorrectly adding encoder pulse number

This case can happen when the motor is hunting around zero speed, including encoder alignment.

=============================================================

if ( directionSample == LL_TIM_COUNTERDIRECTION_DOWN ) {

  /* encoder timer down-counting*/

  OverflowCntSample = ( CntCapture > pHandle->PreviousCapture ) ? 1 : 0;

  pHandle->DeltaCapturesBuffer[pHandle->DeltaCapturesIndex] =

   ( int32_t )( CntCapture ) - ( int32_t )( pHandle->PreviousCapture ) -

   ( ( int32_t )( OverflowCntSample ) + OFbit ) * ( int32_t )( pHandle->PulseNumber );

 }

 =============================================================

(2) no speed reliability check

[ TSK_MediumFrequencyTaskM1() in mc_task.c ]

  • In case of using encoder

=============================================================

__weak void TSK_MediumFrequencyTaskM1(void)

{

...

 (void) ENC_CalcAvrgMecSpeedUnit( &ENCODER_M1, &wAux );

...

 case RUN:

    MCI_ExecBufferedCommands( &Mci[M1] );

  FOC_CalcCurrRef( M1 );

break;

....

}

 =============================================================

  • In case of using hall sensor

=============================================================

__weak void TSK_MediumFrequencyTaskM1(void)

{

...

  bool IsSpeedReliable = HALL_CalcAvrgMecSpeedUnit( &HALL_M1, &wAux );

...

 case RUN:

   MCI_ExecBufferedCommands( &Mci[M1] );

  FOC_CalcCurrRef( M1 );

if( !IsSpeedReliable )

  {

   STM_FaultProcessing( &STM[M1], MC_SPEED_FDBK, 0 );

  }

break;

....

}

 =============================================================

(3) no scheme to clear speed feedback fault once happened

[ SPD_IsMecSpeedReliable() in speed_pos_fdbk.c ]

"ENCODER_M1._Super.bSpeedErrorNumber" is incremented to its max(default:3) then generating an alarm, but no state transition or API to reset this value to zero.

This topic has been closed for replies.

4 replies

THA.1
THA.1Author
Associate III
January 26, 2022

I added additional issues after more test.

THA.1
THA.1Author
Associate III
February 14, 2022

Please could someone ST member clarify this issue?

cedric H
ST Technical Moderator
March 2, 2022

Hello @THA.1​ ,

Thanks for your post.

I do agree with you. We have an issue if we have a speed inversion between two sampling events. This could happen if the motor speed is around 0.

We need to internally check what would be the best way to solve this tricky case.

Regards

Cedric

THA.1
THA.1Author
Associate III
March 3, 2022

Thank you for your reply.

Just a traditional way would be a good choice if sampling frequency is high enough - determining overflow/underflow by the amount of change of the counter.

Regards,

THA.1