Skip to main content
Sune Jensen
Associate II
Sep 25, 2024 6:36 AM UTC
Solved

[Bug report] SPD_GetInstElSpeedDpp only works when using STO+PLL as speed sensing method

 

SPD_GetInstElSpeedDpp is implemented in speed_pos_fdbk.h

 

 

static inline int16_t SPD_GetInstElSpeedDpp(const SpeednPosFdbk_Handle_t *pHandle)
{
#ifdef NULL_PTR_CHECK_SPD_POS_FBK
 return ((MC_NULL == pHandle) ? 0 : pHandle->InstantaneousElSpeedDpp);
#else
 return (pHandle->InstantaneousElSpeedDpp);
#endif
}

 

 

The returned variable pHandle->InstantaneousElSpeedDpp is however only updated when using STO+PLL as speed sensing method (see sto_pll_speed_pos_fdbk.c). For any other method (sensored or sensorless) InstantaneousElSpeedDpp is never updated.

SPD_GetInstElSpeedDpp is used in mc_tasks_foc.c (mc_tasks.c before version 6.3.0) to do do reverse park angle compensation. This means that REV_PARK_ANGLE_COMPENSATION_FACTOR does not work as expected for any other speed sensing method than STO+PLL.

 

 

hElAngle += SPD_GetInstElSpeedDpp(speedHandle)*REV_PARK_ANGLE_COMPENSATION_FACTOR;

 

 

As far as I can figure out, SPD_GetInstElSpeedDpp should actually return pHandle->hElSpeedDpp when using any other method than STO+PLL (or rather the different speed sensing methods ought to be refactored to use the variables in a consistent manner).

This topic has been closed for replies.
GMA
GMABest answer
ST Technical Moderator
Oct 4, 2024 8:20 AM UTC

Hello @Sune Jensen,

Thank you for your problem report. You are fully right; a ticket has been entered on our side and notification will be done once corrected in further delivery.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

2 replies

GMA
GMABest answer
ST Technical Moderator
Oct 4, 2024 8:20 AM UTC

Hello @Sune Jensen,

Thank you for your problem report. You are fully right; a ticket has been entered on our side and notification will be done once corrected in further delivery.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
ST Employee
May 20, 2025 9:36 AM UTC

Hello @Sune Jensen ,

This issue has been fixed with the solution proposed above in our new MCSDK 6.4.0 release,
so feel free to download it and try if it solved correctly your issue reported in this post.

Kind Regards.

If you agree with my answer, please accept it by clicking on 'Accept as solution'.