Associate II
September 30, 2024
Solved
[Bug report] MCM_Modulus does not work for negative alpha values when using CORDIC
- 2 replies
- 1751 views
[VERSION]: 6.3.1
[TOOL]: Firmware
[DETAILS]:
The implementation of MCM_Modulus defined in mc_math.h calls the CORDIC peripheral like this:
LL_CORDIC_WriteData(CORDIC, (((uint32_t)beta << 16U) | (uint32_t)alpha));
This works fine as long as alpha is positive. However, when converting a negative alpha from int16_t to uint32_t the upper 16 bits will all be '1', hence beta is overwritten.
[PROPOSED SOLUTION]:
Mask the upper bits of alpha before combining with beta.
LL_CORDIC_WriteData(CORDIC, (((uint32_t)beta << 16U) | ((uint32_t)alpha & 0xFFFF)));
Note: Images are attached that show calculated phase current using the wrong and the correct conversions respectively.