Skip to main content
Associate III
May 26, 2025 8:28 AM UTC
Solved

Bug MCSDK v6.3.2 - stm32_mc_common_it.c.ftl failed to generate SPD_TIM_M1_IRQHandler

Code generation failed to generate 

void SPD_TIM_M1_IRQHandler(void);

Because the comment section was not closed off with "-->"

 

Line 171 in stm32_mc_common_it.c.ftl: 

<#else> <#--CondFamily_STM32F0 || CondFamily_STM32F4 || CondFamily_STM32F7 || CondFamily_STM32F3 || CondFamily_STM32G4 || CondFamily_STM32H5 || CondFamily_STM32H7 || CondFamily_STM32L4>
 <#if (M1_ENCODER == true) >
void SPD_TIM_M1_IRQHandler(void);

 Needs to be: 

<#else> <#--CondFamily_STM32F0 || CondFamily_STM32F4 || CondFamily_STM32F7 || CondFamily_STM32F3 || CondFamily_STM32G4 || CondFamily_STM32H5 || CondFamily_STM32H7 || CondFamily_STM32L4 -->
 <#if (M1_ENCODER == true) >
void SPD_TIM_M1_IRQHandler(void);

 
Error is only apparent when both Encoder and Hall sensor are used because of the double function name SPD_TIM_M1_IRQHandler 

This topic has been closed for replies.
GMA
GMABest answer
ST Technical Moderator
May 26, 2025 3:16 PM UTC

Hello @Zeno,

Thank you for your report.
Encoder/Hall speed sensing configuration has not been taken into account as usually Encoder and Hall are connected through the same input pins.
Using Main sensor set to Encoder and Auxiliary sensor set to Hall and renaming 

SPD_TIM_M1_IRQHandler to SPDEnc_TIM_M1_IRQHandler/SPDHall_TIM_M1_IRQHandler according to TIM IP feature connection, it should be ok. 
If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

2 replies

GMA
GMABest answer
ST Technical Moderator
May 26, 2025 3:16 PM UTC

Hello @Zeno,

Thank you for your report.
Encoder/Hall speed sensing configuration has not been taken into account as usually Encoder and Hall are connected through the same input pins.
Using Main sensor set to Encoder and Auxiliary sensor set to Hall and renaming 

SPD_TIM_M1_IRQHandler to SPDEnc_TIM_M1_IRQHandler/SPDHall_TIM_M1_IRQHandler according to TIM IP feature connection, it should be ok. 
If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
ZenoAuthor
Associate III
May 31, 2025 1:42 PM UTC

Hi GMA, 

Yea I figured just renaming te function prototypes was fine, thanks!