Skip to main content
KSzul.1
Associate II
August 14, 2022
Question

Bug in Motor Pilot V0.9.20 from ST MCW 5.Y.4.21553 Rev-up Phases Configuration?

My setup:

NUCLEO-F446RE and STEVAL-IPM15B

"ST Motor Control Workbench" "Power Stage - Current Sensing" settings:

  • Shunt resistors value: 0.04 Ohm (also on PCB, but User Manual um-2014-1500-... says 0.08 ohm, another mismatch)
  • Amplifying network gain: 2.10
  • T-rise: 1500
  • T-noise: 2000

These values are in "power_stage_parameters.h" too.

However, Motor Pilot in "Rev-up" tab, "Phases configuration" -> click "Read all", reads as follows:

  • RShunt: 0.0050 ohm
  • OPAMP Gain: 24
  • Vref: 3.3 V

That effectively lowers down current/torque about 30% in rev-up phase.

Is it a bug or a feature? Motor Pilot does not read RShunt and gain values from the firmware?

Thank you.

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
August 25, 2022

Hello,

"Read all" corresponds to full fill the "Phase configuration" table only. If you want to display the table in "Amp" format and not in "S16A" format, you have to enter manually the "Rshunt" box values in order to have a correct conversion.

Best regards.

GMA

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA