Skip to main content
Sun1
Associate
September 30, 2021
Solved

BR2804 motor 1700kv-1, parameters or datasheet. I am using P-NUNCLEO-IHM001 package(nucleo-F302R8, STSPIN L6230 motor driver, BR2804 motor 1700kv-1) to performance FOC algorithm.

hello, I am using P-NUNCLEO-IHM001 package(nucleo-F302R8, STSPIN L6230 motor driver, BR2804 motor 1700kv-1) to performance FOC algorithm. But i did not find Parameters of the motor, could someone let me know where can i find the datasheet or Details of parameters of the motor. thanks

This topic has been closed for replies.
Cristiana SCARAMEL
ST Employee
October 12, 2021

Hi @Sun​ and welcome to the ST Community.

If you use the STM32 Motor Control Software Development Kit (X-CUBE-MCSDK) you can find the motor Bull Running BR2804-1700kv in the drop down list (when you create a New Project).

0693W00000FCBZVQA5.png 

Otherwise you can use the available Project example for P-NUCLEO-IHM001 (3-shunt, sensorless).

In both cases you can find the Motor Parameters needed.

0693W00000FCBraQAH.png 

Let me know if my reply fully answered your question, if so please "Select as Best" label.

"If you feel a post has answered your question, please click ""Accept as Solution"""

2 replies

Sun1
Sun1Author
Associate
October 1, 2021

BR2804 motor 1700kv-1

Cristiana SCARAMEL
ST Employee
October 12, 2021

Hi @Sun​ and welcome to the ST Community.

If you use the STM32 Motor Control Software Development Kit (X-CUBE-MCSDK) you can find the motor Bull Running BR2804-1700kv in the drop down list (when you create a New Project).

0693W00000FCBZVQA5.png 

Otherwise you can use the available Project example for P-NUCLEO-IHM001 (3-shunt, sensorless).

In both cases you can find the Motor Parameters needed.

0693W00000FCBraQAH.png 

Let me know if my reply fully answered your question, if so please "Select as Best" label.

"If you feel a post has answered your question, please click ""Accept as Solution"""