Skip to main content
ST Employee
Oct 17, 2023 1:32 PM UTC
StickyQuestion

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enable users to configure their motor-control application and produce a software project that implements it following its hardware component features. 

Wiki Link


A new documentation will arrive soon and will detail these features: 

  • Current Sensing: three-shunt-raw-currents-differential-internal-opamp-with-external-gain-and-filtered-adc-intput-hwv 

  • ICS 

  • Phase Voltage sensing feature 

  • Driver Protection feature 

The descVersion property is equal to 4 from version 6.2.0 of the MCSDK and the "contentVersion" property is added.

For questions regarding the board manager, please respond under this post.

 

Regards

This topic has been closed for replies.

5 replies

Visitor II
Oct 20, 2023 1:48 PM UTC

Hi Zied,

good news... we appreciate configuring our custom boards more easily...

However, when we are looking on version 6.2 we don't see the window as shown in the wiki see attached.

Thanks in advance for helping us.

Kind Regards#

Guenther

here the doc window: 

Gboost_0-1697809593317.png

 

thats what we are seeing on 6.2 

Gboost_1-1697809671742.png

 

 

Zied b.Author
ST Employee
Oct 24, 2023 12:18 PM UTC

hi @Gboost ,
The interface changes a little, but the parameters remain the same, the same functionalities are offered to the user.
Regards

"If you agree with my answer, please accept it by clicking on ""Accept as solution""."
DMeie.2
Associate III
Dec 20, 2023 10:29 AM UTC

What's the ETA on descVersion 4 of the documentation?

Associate III
Oct 26, 2024 6:52 AM UTC

Where can i find STEVAL-ESC001V1 in MCSDK ? 

GMA
ST Technical Moderator
Oct 28, 2024 3:57 PM UTC

Hello @tejas_amp,

Please, do not use an old post to add a new question. 
Creating a new post prevents to sending messages to all users thread. STEVAL-ESC001V1 is available in Inverter tab.

GMA_0-1730130963263.png

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA