Skip to main content
DMeie.2
Associate III
February 28, 2024
Solved

Board Manager "busVoltageDivider" issues

I'm having issues with the "busVoltageDivider" property in the "VBusSensing" feature.

The Wiki says that the "VBusSensing" feature doesn't define any global propery, however the Board Manager is complaining that the property is missing when I don't add it.

Furthermore, how is this and the "busVoltageDivider" property inside the "VBusSensing" hardware type (I'm assuming they're identical) calculated?
The other properties "busVoltageDividerR1" and "busVoltageDividerR2" are obvious.

This topic has been closed for replies.
Fred V.
Fred V.Best answer
ST Employee
March 5, 2024

Hello @DMeie.2 ,

 

Indeed, there is an error in the implementation that do not conform to the specification. The Workbench and the Board Manager mandate that the busVoltageDivider property be defined both at feature and at hardware variant level. Both properties have the same value as they represent the same thing.  This issue will be corrected in a future release. 

 

You also unveiled another error, in the wiki this time: in the figure that sketches the implementation of the VBusSensing hardware variant, R1 and R2 should be switched. Then, the busVoltageDivider is computed as (R1+R2)/R2.  This issue will be fixed shortly in the Wiki.

 

Best Regards,

 

FredV

 

1 reply

Fred V.
Fred V.Best answer
ST Employee
March 5, 2024

Hello @DMeie.2 ,

 

Indeed, there is an error in the implementation that do not conform to the specification. The Workbench and the Board Manager mandate that the busVoltageDivider property be defined both at feature and at hardware variant level. Both properties have the same value as they represent the same thing.  This issue will be corrected in a future release. 

 

You also unveiled another error, in the wiki this time: in the figure that sketches the implementation of the VBusSensing hardware variant, R1 and R2 should be switched. Then, the busVoltageDivider is computed as (R1+R2)/R2.  This issue will be fixed shortly in the Wiki.

 

Best Regards,

 

FredV