Skip to main content
Visitor
Jul 23, 2026 3:28 PM UTC
Solved

BLDC Motor controller with encoder interface

Hello,

I am looking for a BLDC motor controller with Hall sensor and Encoder interface. Hall sensor is used for commutation and Encoder will be used for position control. I could not find a motor controller with above mentioned interface. 

Can you suggest a suitable controller?

Thanks,

Anand

GMA
GMABest answer
ST Technical Moderator
Jul 24, 2026 7:18 AM UTC

Hello ​@Anand369,

The majority of inverters or power boards have one connector used for encoders or Hall sensors.
EVLSERVO1 inverter board or STDES-LVHP01/STEVAL-LVLP01 power boards have two connectors to manage Encoder and Hall sensors at the same time.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

1 reply

GMA
GMABest answer
ST Technical Moderator
Jul 24, 2026 7:18 AM UTC

Hello ​@Anand369,

The majority of inverters or power boards have one connector used for encoders or Hall sensors.
EVLSERVO1 inverter board or STDES-LVHP01/STEVAL-LVLP01 power boards have two connectors to manage Encoder and Hall sensors at the same time.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA