Skip to main content
Associate II
Mar 18, 2026 12:02 PM UTC
Question

BLDC: Delete the Alignment phase of the encoder

Hi all,

I noticed that when using the encoder, the motor undergoes an alignment phase during which it completes a rotation until it reaches the position where the Index Z signal is triggered.

I was wondering if it's possible to skip this alignment phase by adding the Hall sensors (like with the B-G473E combined with the STEVAL-LVLP01 board), and if so, what should I specify in the Workbench or in the Code?

Regards,
Jules

3 replies

GMA
ST Technical Moderator
Mar 19, 2026 8:01 AM UTC

Hello @JulesC,

As mentioned in the Alignment settings chapter of the User manual Quadrature Encoder sensor feedback processing documentation, absolute information is required to perform field-oriented control. Therefore, it cannot be skipped in the current MCSDK implementation.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
JulesCAuthor
Associate II
Mar 23, 2026 3:23 PM UTC

Hello @GMA,
Sorry for the late reponse.
Is it possible for the Quadrature Encoder to determine the absolute information using Hall sensors? For instance, could the system start in Hall sensor mode and then switch to the Quadrature Encoder once the index is found or the position is synchronized?

Regards,
Jules

GMA
ST Technical Moderator
Apr 13, 2026 8:57 AM UTC

Hello @JulesC,

In the current MCSDK implementation, the speed sensor switch is available, however, for the Encoder sensor, alignment is required.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA