Skip to main content
Raphael_Ko
Associate II
Jan 8, 2026 7:54 PM UTC
Solved

B-G473E-ZEST1S with MCSDK 6.4.1 singnal handler after startup

Hallo,
i try to run an B-G473E-ZEST1S with STEVAL-LVLP01A. I generate code with the default setting from MCSDK 6.4.1., STM32CubeMX 6.16.1, STM32 FW V1.6.1 (Recommended)

I changed nothing on the board hardware or MCSDK settings, i choose the 2 boards and generate code, but after startup I end always in an "<signal handler called at 0xffffffe9>".

The error occours after MX_NVIC_Init(); without MX_NVIC_Init(); the code is running, so it has something to do with the interrupts, but I don't get it.
Does anyone know what could be the cause of this error? Has anyone successfully used this board with the MCSDK 6.4.1?

Thank you!

Raphael_Ko
Raphael_KoBest answer
Associate II
Jan 8, 2026 9:57 PM UTC

I have found it, it was the missing boot 0 jumper on the board.

2 replies

Raphael_Ko
Raphael_KoAuthorBest answer
Associate II
Jan 8, 2026 9:57 PM UTC

I have found it, it was the missing boot 0 jumper on the board.

GMA
ST Technical Moderator
Jan 12, 2026 12:48 PM UTC

Hello @Raphael_Ko,

Thank you for your feedback.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA