Skip to main content
SRedd.5
Senior III
June 4, 2023
Solved

B-G431B-ESC1 software and motor parameters Rs, Inductance.

When i refer the source code of the B-G431B-ESC1 board, i do not see the code check for series resistance, inductance of the motor. Is the source code independent of the series and inductance of the motor? For example

/***************** MOTOR ELECTRICAL PARAMETERS ******************************/

#define RS           0.35 /* Stator resistance , ohm*/

#define LS           0.0006 /* Stator inductance, H

But i do not see these parameters used anywhere in the program. Is my understanding correct?

This topic has been closed for replies.
JKong.3
JKong.3Best answer
Associate III
June 26, 2023

it's in Inc/pmsm_motor_parameters.h

1 reply

JKong.3
JKong.3Best answer
Associate III
June 26, 2023

it's in Inc/pmsm_motor_parameters.h