Skip to main content
Visitor II
March 18, 2024
Question

b-g431b-esc1 BLDC

To whom it may concern,

 

I am developing a controller for BLDC, I managed to initialize the board with cubeIDE and flash code (so far only turning on the LED).

 

However, I need to use a BLDC motor for my project and I have searched everywhere on how to initialize and do a motor profiler, etc. But there is no information about how it works, just that it doesn't.

 

Could you please provide information on how to set up the 6-step controller with b-g431b-esc1 and which software should be used, since so far none of your released software works. 

 

This is the BLDC motor I am using: https://maytech.cn/products/mto5065-170-ha-c

 

Any help would be appreciated.

 

Sincerely,

Mykolas

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
March 19, 2024

Hello,

Please use STM32 Motor Control Software Development Kit tool.
User manual UM3027 How to use STM32 motor control SDK v6.0 workbench available here.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA