Skip to main content
Associate
November 9, 2024
Question

B-G431B-ESC1 6-step algorithm

I have an A2212 13T motor with B-G431B-ESC1 with  6-step trapezoidal algorithm.It is tracking the speed reference input.

But the problem is that it takes time to reach the desired speed.Suppose currently my motor speed is at 5000 rpm, but if I change the speed to 8000 rpm, it takes time to reach that speed.How to overcome that problem?

 

This topic has been closed for replies.

2 replies

November 10, 2024

Hey @sambit_das  

You must change the speed PI parameters and fine tune them to fit best for your application

Regards!

Gael A
ST Employee
November 11, 2024

Hello sambit_das,

In addition to what MotorRunner said, I would also recommend you to check your speed ramp value and increase it if need be.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.