Skip to main content
JLax
Visitor II
September 27, 2018
Question

Atollic error "cannot find -l:libmc-truestudio_M0.lib" with STEVAL-SPIN3201

  • September 27, 2018
  • 1 reply
  • 557 views

I am using the Motor control Workbench 5.1.0.18254 to generate an Atollic project for SPIN3201 eval board. When I try to generate the project, it does not find the following library "cannot find -l:libmc-truestudio_M0.lib".

I think the problem is that this library is not in the repository that generates the project "C:\Users\***\STM32Cube\Repository\MCSDK_v5.1.2-A1\MotorControl\lib".

Do I need to update the Motor Control Workbench application?

Best Regards

Jorge

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards