Skip to main content
BAbde.1
Associate
April 23, 2020
Solved

ACIM motor

Have Nucleo-64 STM32L476RG and STEVAL-IPM15B , i plan to test VFD and FOC drive for pump with ACIM motors , but the workbench motor control is for pemanent magnetic motor !!

are there any additional library or sdk to handle ACIM motor ?

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
June 28, 2021

Dear @BAbde.1​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

3 replies

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Laurent Ca...Best answer
Senior III
June 28, 2021

Dear @BAbde.1​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

BAbde.1
BAbde.1Author
Associate
July 21, 2021

thanks alot , where i can dowload it please ?