Skip to main content
LLion.1
Visitor II
November 17, 2022
Question

About FOC generated code with MCSDK

I am a newer leraning motor FOC control. I study the generated code by MCSDK tool with hall (120 degree). Below is some question:

  1. In file mc_config.c, about hall configuration ".hMaxReliableMecSpeedUnit     = (uint16_t)(1.15*MAX_APPLICATION_SPEED_UNIT),". Here why need to times 1.15?
  2. In file mc_parameters.c, about ADC configuration, as below

.ADCConfig1 = {  MC_ADC_CHANNEL_11<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_10<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_10<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_10<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_10<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_11<<ADC_JSQR_JSQ4_Pos

         },

​

 .ADCConfig2 = {  MC_ADC_CHANNEL_12<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_12<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_12<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_11<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_11<<ADC_JSQR_JSQ4_Pos

          ,MC_ADC_CHANNEL_12<<ADC_JSQR_JSQ4_Pos

         },

​

 .ADCDataReg1 = { &ADC1->JDR1 /* Phase B, Phase C */

          ,&ADC1->JDR1 /* Phase A, Phase C */

          ,&ADC1->JDR1 /* Phase A, Phase C */

          ,&ADC1->JDR1 /* Phase A, Phase B */

          ,&ADC1->JDR1 /* Phase A, Phase B */

          ,&ADC1->JDR1 /* Phase B, Phase C */

         },

​

 .ADCDataReg2 = { &ADC2->JDR1 /* Phase B, Phase C */

          ,&ADC2->JDR1 /* Phase A, Phase C */

          ,&ADC2->JDR1 /* Phase A, Phase C */

          ,&ADC2->JDR1 /* Phase A, Phase B */

          ,&ADC2->JDR1 /* Phase A, Phase B */

          ,&ADC2->JDR1 /* Phase B, Phase C */

        },

why each channel is set in JSQ4? But in ADCx_Init(), the channels for phaseABC are set in JSQ234.

When read each phase ADC conversion result, why read JDR1? According to ADC init, should be JDR234.

This topic has been closed for replies.