Skip to main content
Associate II
Nov 14, 2025 5:11 AM UTC
Solved

6-Step Algorithm for Sensorless Motor application

I am using the STM32 NUCLEO-G474RE control board and the NUCLEO-IHM08M1 inverter board for a motor-control application. I want to run a 6-step (trapezoidal) commutation algorithm, so I need to generate PWM signals from the control board to the driver IC on the power board(NUCLEO-IHM08M1).

The driver IC (L6398) truth table specifies:

  • HIN = 0 and LIN = 0 → Low-side ON

  • HIN = 1 and LIN = 1 → High-side ON

But the STM32 timer provides complementary PWM outputs, where each channel only gives PWM + its inverted output, so it does not match the L6398 input logic. With complementary channels, the outputs are only HIGH or LOW for PWM—they cannot give “both HIGH” or “both LOW” on the same phase simultaneously as required by the driver.

Therefore, I need guidance on how to generate the correct 6-step commutation sequence for the IHM08M1 board using the NUCLEO-G474RE, given that the L6398 requires both HIN and LIN to be controlled independently.

Fabrice LOUBEYRE
Fabrice LOUBEYREBest answer
ST Employee
Nov 17, 2025 2:38 PM UTC

Hi @Esakkimuthu,

 

MCSDK 6.4.1 controls complementary PWM generation on high-side and low-side signals for phase control with the specified board configuration.

To modify the management, you must directly change the code of the MCSDK.

After generating a project with the MCSDK workbench, the file mc_parameters.c contains several definitions for the PWM timer, particularly configurations for the CCER, CCMR1, and CCMR2 registers. These registers control the states of the PWM high-side and low-side signals.

Refer to the register description in chapter 29, Advanced-control timers (TIM1/TIM8/TIM20), of the documentation available at:

https://www.st.com/resource/en/reference_manual/rm0440-stm32g4-series-advanced-armbased-32bit-mcus-stmicroelectronics.pdf

For example, you can update the following structures according to your requirements.

.CCER_cfg = {
CCER_STEP14_CUSTOM,
CCER_STEP25_CUSTOM,
CCER_STEP36_CUSTOM,
CCER_STEP14_CUSTOM,
CCER_STEP25_CUSTOM,
CCER_STEP36_CUSTOM,
},

 

.CCMR1_Standard_cfg = {
CCMR1_STEP1_CUSTOM,
CCMR1_STEP2_CUSTOM,
CCMR1_STEP3_CUSTOM,
CCMR1_STEP4_CUSTOM,
CCMR1_STEP5_CUSTOM,
CCMR1_STEP6_CUSTOM,
},
.CCMR2_Standard_cfg = {
CCMR2_STEP1_CUSTOM,
CCMR2_STEP2_CUSTOM,
CCMR2_STEP3_CUSTOM,
CCMR2_STEP4_CUSTOM,
CCMR2_STEP5_CUSTOM,
CCMR2_STEP6_CUSTOM,
},

In your case something like that:

  • Phase A: HIN_A = PWM, LIN_A = 1

  • Phase B: HIN_B = 0, LIN_B = 0

  • Phase C: HIN_C = 0, LIN_C = 1

#define CCER_STEP14_CUSTOM  TIM_CCER_CC4E_Msk | TIM_CCER_CC3NE_Msk | TIM_CCER_CC3E_Msk | TIM_CCER_CC2NP | TIM_CCER_CC2NE_Msk | TIM_CCER_CC1NP | TIM_CCER_CC1E_Msk, /* A B */

#define  CCMR1_STEP1_CUSTOM  TIM_CCMR1_OC2M_2 | TIM_CCMR1_OC2M_0 | TIM_CCMR1_OC2PE_Msk | TIM_CCMR1_OC1M_2 | TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1PE_Msk, /* */

#define CCMR2_STEP1_CUSTOM TIM_CCMR2_OC4M_2 | TIM_CCMR2_OC4M_1 | TIM_CCMR2_OC4PE_Msk | TIM_CCMR2_OC3M_2 | TIM_CCMR2_OC3PE_Msk, /* */

....

 

Best regards.

Fabrice

5 replies

Senior III
Nov 14, 2025 7:11 AM UTC

STuser2_0-1763104187817.png

STuser2_1-1763104216433.png

 

LIN is active low input, whether you have considered this?

 

Associate II
Nov 14, 2025 9:24 AM UTC

Yes, I have considered that LIN is active-LOW.
The L6398 truth table requires the inputs to be equal to turn a MOSFET ON:

  • HIN = 1, LIN = 1 → High-side ON

  • HIN = 0, LIN = 0 → Low-side ON

  • HIN = 0, LIN = 1 → Phase FLOAT (both OFF)

So for low-side ON I must drive LIN = 0, and for high-side ON I must drive LIN = 1.

My practical control scheme:

  • Phase HIGH: HIN = PWM, LIN = 1

  • Phase LOW: HIN = 0 (PWM disabled), LIN = 0

  • Phase FLOAT: HIN = 0, LIN = 1

I will not use the complementary CHxN outputs because they generate the opposite of HIN and would create invalid 1/0 → OFF states.

This approach is correct for 6-step BLDC where:

  • PWM is applied only on the high-side of the active phase, and

  • the low-side of the sink phase remains fully ON (LIN = 0) during the entire step.

Example:
To drive A+ / B- / C floating

  • Phase A: HIN_A = PWM, LIN_A = 1

  • Phase B: HIN_B = 0, LIN_B = 0

  • Phase C: HIN_C = 0, LIN_C = 1

Senior III
Nov 14, 2025 9:49 AM UTC

I am not sure how you are generating the code etc, but see if the below CubeMx settings are useful

STuser2_0-1763113682927.png

It is giving an option to generate complementary or independent, verify if it is useful.