Skip to main content
Associate II
Nov 14, 2025 8:50 AM UTC
Solved

zephyr stm32u5g9j-dk2 adc not function

Hello, I am using the Zephyr operating system with the STM32U5G9J-DK2 hardware. I intend to collect voltage data using the ADC, but so far, no progress has been made. Here are the steps I have taken:
  • I used the zephyr\samples\drivers\adc\adc_sequence example from Zephyr 4.2.0.
  • I created a new app.overlay file in the root Vmakelists.txt directory with the following content:
    / {
     aliases {
     adc0 = &adc1;
     };
    };
    
    &vbat1 {
     status = "okay";
     io-channels = < &adc1 5 >;
    };
     
  • I compiled using this command:west build -p always -b stm32u5g9j_dk2 --sysbuild .
  • Then I supplied 1V to the PA0 pin (silkscreen labeled PWM/D6), and the log is as follows:
  •  
     
[16:22:28.487] RX←◆*** Booting Zephyr OS build v4.2.0 ***ADC sequence reading [0]:
[16:22:29.493] RX←◆- adc@42028000, channel 5, 5 sequence samples:

2684 = 2162mV

1788 = 1440mV

1571 = 1265mV

1532 = 1234mV

1492 = 1202mV

adc@42028000, channel 12, 5 sequence samples:

2092 = 1685mV

1660 = 1337mV

1571 = 1265mV

1532 = 1234mV

1532 = 1234mV

  • Subsequently, I changed the supply voltage to 2V, and the log is as follows:[16:27:39.509] RX←◆- adc@42028000, channel 5, 5 sequence samples:

0 = 0mV

1068 = 860mV

1404 = 1131mV

1492 = 1202mV

1492 = 1202mV

adc@42028000, channel 12, 5 sequence samples:

636 = 512mV

1315 = 1059mV

1492 = 1202mV

1492 = 1202mV

1532 = 1234mV

No significant changes are observable. I also tried the example in samples\boards\st\power_mgmt\adc\src\main.c, but still cannot obtain correct results. Could you please advise on how to acquire accurate ADC values using Zephyr?
gautierg-stBest answer
ST Employee
Nov 17, 2025 2:03 PM UTC

Hello @devin-hu,

I've tested on my side and I got the same results as you. I've fixed it by changing the value of `<st,adc-prescaler>` value to 2 instead of 1 in the board dts file.

I've pushed a PR on Github to fix this issue here: boards: st: stm32u5g9j_dk: adjust adc prescaler by gautierg-st · Pull Request #99506 · zephyrproject-rtos/zephyr.

Hope this helps.

2 replies

gautierg-stBest answer
ST Employee
Nov 17, 2025 2:03 PM UTC

Hello @devin-hu,

I've tested on my side and I got the same results as you. I've fixed it by changing the value of `<st,adc-prescaler>` value to 2 instead of 1 in the board dts file.

I've pushed a PR on Github to fix this issue here: boards: st: stm32u5g9j_dk: adjust adc prescaler by gautierg-st · Pull Request #99506 · zephyrproject-rtos/zephyr.

Hope this helps.

devin-huAuthor
Associate II
Nov 25, 2025 8:52 AM UTC

Hi,

Thank you for your reply. This solution is effective.