Skip to main content
ZZida.1
Associate II
Sep 4, 2020 8:31 AM UTC
Solved

xQueueSendFromISR hangs out application [SOLVED]

Hi All,

I use FreeRTOS and I try to use USART by interrupt. When I call xQueueSendFromISR my application hangs out. I've set full assert but it never reaches assert_failed or Error_Handler functions.

I use NUCLEO-64 STM32F411RE board with 1.25.0 firmware package and STM32 CubeIDE 1.4.0. from Linux.

Here is the interrupt code :

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
 if (huart == &huart2) {
 sh_receive_complete(huart);
 return;
 }
}
 
/**
 * receive completed interrupt function
 */
void sh_receive_complete(UART_HandleTypeDef *huart) {
	BaseType_t hptw = pdFALSE;
 
	if (!(huart && huart == configuration->uart))
		return;
 
	xQueueSendFromISR(receive_queue, &receive_buffer, &hptw);
	HAL_UART_Receive_IT(configuration->uart, &receive_buffer, 1U);
}

when this code reached xQueueSendFromISR never come back.

My FreeRTOS config params:

#ifndef FREERTOS_CONFIG_H
#define FREERTOS_CONFIG_H
 
 
/* Ensure definitions are only used by the compiler, and not by the assembler. */
#if defined(__ICCARM__) || defined(__CC_ARM) || defined(__GNUC__)
 #include <stdint.h>
 extern uint32_t SystemCoreClock;
#endif
#define configENABLE_FPU 0
#define configENABLE_MPU 0
 
#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 1
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 56 )
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)15360)
#define configMAX_TASK_NAME_LEN ( 16 )
#define configUSE_TRACE_FACILITY 1
#define configUSE_16_BIT_TICKS 0
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 8
#define configUSE_RECURSIVE_MUTEXES 1
#define configUSE_COUNTING_SEMAPHORES 1
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 0
 
#define configMESSAGE_BUFFER_LENGTH_TYPE size_t
 
/* Co-routine definitions. */
#define configUSE_CO_ROUTINES 0
#define configMAX_CO_ROUTINE_PRIORITIES ( 2 )
 
/* Software timer definitions. */
#define configUSE_TIMERS 1
#define configTIMER_TASK_PRIORITY ( 2 )
#define configTIMER_QUEUE_LENGTH 10
#define configTIMER_TASK_STACK_DEPTH 256
 
/* Set the following definitions to 1 to include the API function, or zero
to exclude the API function. */
#define INCLUDE_vTaskPrioritySet 1
#define INCLUDE_uxTaskPriorityGet 1
#define INCLUDE_vTaskDelete 1
#define INCLUDE_vTaskCleanUpResources 0
#define INCLUDE_vTaskSuspend 1
#define INCLUDE_vTaskDelayUntil 1
#define INCLUDE_vTaskDelay 1
#define INCLUDE_xTaskGetSchedulerState 1
#define INCLUDE_xEventGroupSetBitFromISR 1
#define INCLUDE_xTimerPendFunctionCall 1
#define INCLUDE_xQueueGetMutexHolder 1
#define INCLUDE_uxTaskGetStackHighWaterMark 1
#define INCLUDE_eTaskGetState 1
 
#define USE_FreeRTOS_HEAP_4
 
/* Cortex-M specific definitions. */
#ifdef __NVIC_PRIO_BITS
 /* __BVIC_PRIO_BITS will be specified when CMSIS is being used. */
 #define configPRIO_BITS __NVIC_PRIO_BITS
#else
 #define configPRIO_BITS 4
#endif
 
#define configLIBRARY_LOWEST_INTERRUPT_PRIORITY 15
 
#define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY 5
 
#define configKERNEL_INTERRUPT_PRIORITY 		( configLIBRARY_LOWEST_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )
#define configMAX_SYSCALL_INTERRUPT_PRIORITY 	( configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )
 
 
#define configASSERT( x ) if ((x) == 0) {taskDISABLE_INTERRUPTS(); for( ;; );}
 
#define vPortSVCHandler SVC_Handler
#define xPortPendSVHandler PendSV_Handler
 
 
#define xPortSysTickHandler SysTick_Handler
 
#endif /* FREERTOS_CONFIG_H */

thx,

Zamek

This topic has been closed for replies.
ZZida.1
ZZida.1Best answer
Associate II
Sep 4, 2020 9:20 AM UTC

I found the solution:

need to set preemption priority of USART to 15

1 reply

ZZida.1
ZZida.1AuthorBest answer
Associate II
Sep 4, 2020 9:20 AM UTC

I found the solution:

need to set preemption priority of USART to 15