Skip to main content
John886
Associate II
October 25, 2019
Solved

X-CUBE-USB-PD VDM issue on FUSB307BGEVB

  • October 25, 2019
  • 13 replies
  • 3237 views

Act as the DFP. I request the PE to send SOP identify request to the UFP after PE received the data it didn't fire the callback function. (I set the breakpoint at fusb305_tcpc_get_message and i see the data received from the DFP is correct.)

But

  1. when i request the PE to send SOP SVID request to the DFP it did fire the callback function.
  2. when i request the PE to send SOP' identify request to the cable it did fire the callback function.

I'm not sure if i set the configuration correct or there is any problem in the usb pd library.

Thanks.

John

This topic has been closed for replies.
Best answer by Yohann M.

Dear @John886​ 

Please find all the libs generated with VDM patch.

For the 2nd question, I would prefer keeping the other thread already opened by you :

=> https://community.st.com/s/question/0D50X0000BaN2XpSQK/pnucleousb002-cant-recognize-the-emarker-cable

Regards,

Yohann

Note: For your information, we posted an update of X-CUBE-USBPD under github (V3.1.0):

=> https://github.com/STMicroelectronics/x-cube-usb-pd

13 replies

Yohann M.
ST Employee
October 28, 2019

Hello,

Project 'EVAL_FUSB307_DRP' delivered with 'STM32CubeExpansion_USBPD_F0_V2.1.0' does not have the VDM option enabled.

User Manual UM2552 explains the different libs delivered with FW package:

0690X00000ArKghQAF.jpg

It means that you have to:

  • select USBPDTCPM_PD3_FULL_CM0_wc32.a in your workspace (instead of USBPDTCPM_PD3_CONFIG_1_CM0_wc32.a)
  • enable swich USBPD_TCPM_LIB_PD3_FULL (instead of USBPD_TCPM_LIB_PD3_CONFIG_1)

(you can refer to Consumer_VDM_RTOS application which enables VDM by default)

To help you, I updated the project to enable VDM and import usbpd_vdm_user files which allows to implement different VDM callbacks.

For your information, I also enabled _TRACE in this project to allow to evacuate traces over USART pins (PA0 & PA1) connected in my side to VCP used in ST-Link.

Further details described in another post:

"in the projects we deliver, the internal trace is enabled. It is possible to see if you have communication between 2 boards.

Trace is done through USART pins connected to ST link. You should use Cubemonitor-UCPD and use the functionality described in the following image:

0690X00000ApRTRQA3.png

"

Regards,

Yohann

John886
John886Author
Associate II
October 31, 2019

Hi Yohann

Thanks for your help.

I followed your step but the problem is the same when mcu received the VDM message from the partner port, UPF, it didn't call the callback function USBPD_VDM_InformIdentity.

It is the screenshot of the STM32CudeMonirot USB Type-C PD shows PE actually received the message.

0690X00000ArTpYQAV.png

BR

John.

Dominique
ST Employee
October 31, 2019

​Hi John

I'm a colleague of Yohann working on type C. I think your issue could be link with the request mechanisme implemented within our USB-PD stack.

Our USB-PD stack allows to send request but only one at a time. Therefore, if a request is ongoing and you try to post a second request, the stack will reply USBPD_BUSY. This means that the request has not been taken into account by the stack because there is already a pending request. So you shall wait the request completion before to send a new one.

The function USBPD_PE_SVDM_RequestIdentity could repply USBPD_ERROR if there is mismatch within the conditions to send this kind of request

The conditions are the following:

               the feature PE_AttemptsDiscovSOP has been enabled inside the usbpd_conf.h

               there is VDM_Callback

                request is SOP or SOP'

               no ongoing request (USBPD_BUSY)

               there in an explicit contract bewteen the both ports partner or the port is SRC and providing 5V

Please could you check the return of the function USBPD_PE_SVDM_RequestIdentity ?

Another important thing, any discussion with the cable implies that you must power VCONN otherwise the component inside the cable is not powered and can not answer to a message.

BR

Dominique.

John886
John886Author
Associate II
November 1, 2019

Hi Dominique

Thanks for your reply.

I enable the VDM, VCONN_SUPPORT, USBPD_TCPM_LIB_PD3_FULL and link the library to USBPDTCPM_PD3_FULL_CM0_wc32.

This is my DPM_Settitng0690X00000ArWosQAF.png

The below is my debug process​. 

I use fusb307evb and configure it to

  1. Datarole is UFP
  2. Port type is sink.

0690X00000ArWpgQAF.png

1.Sop_1

When i called the USBPD_PE_SVDM_RequestIdentity(PortNum,SOP'), i got the VDM message replied by the e-marker of the cable.

The figures shows VDM message received by usb305 is consistent with what ez_pd, EZ-PD™ Protocol Analyzer for cypress, read then the PE calls the callback function.

0690X00000ArWp2QAF.png0690X00000ArWp7QAF.png

0690X00000ArWpCQAV.png

2. SOP

When i called the USBPD_PE_SVDM_RequestIdentity(PortNum,SOP), i got the VDM message replied by the partner port.

The figures shows the VDM message usb305 received is consistent with what ez_pd, EZ-PD™ Protocol Analyzer for cypress, read.

The return value o the USBPD_PE_SVDM_RequestIdentity(PortNum,SOP) is USBPD_TRUE but this time PE didn't call the callback after receiving the VDM message.

0690X00000ArWpRQAV.png

0690X00000ArWpMQAV.png0690X00000ArWpHQAV.png

I'm not sure if i can retrieve the VDM message from the callback function called by the PE after receiving the correct VDM message replied by partner port after calling USBPD_PE_SVDM_RequestIdentity or i need to call another function to retrieve it.

Thanks.

BR.

John

Yohann M.
ST Employee
November 5, 2019

Dear John,

In our stack, we check the content validity of the Discovery identity and we had an issue in this check (fixed in our latest delivery done for our G0 series). I updated the lib used in your environment. Could you please try it and let me know if it works or not? (I tested in my side, it should be OK ;) )

Regards

Yohann

John886
John886Author
Associate II
November 6, 2019

Dear Yohann

I used the library you uploaded yesterday, the weird thing happened.

The block in black is the old library that x-cude pd provide and the block in red is the new library you provided.

0690X00000ArjTdQAJ.png

when i used the new library.

After receiving the hard reset sent by the fusb307evb , mcu hanged on the hard fault

Could you please provide the project that worked well in your side.

Thanks.

BR.

John

Yohann M.
ST Employee
November 7, 2019

Dear John,

Library I delivered is a library to be used on IAR or SW4STM32 (*_wc32.a libs).

For Keil, you should use *_keil.lib libs.

Please use the attached zip file in which one the lib for keil is available.

Regards,

Yohann

John886
John886Author
Associate II
November 12, 2019

Dear @Yohann M.​ 

I found the same issue in :USBPDCORE_PD2_FULL_CM0_wc32 and :USBPDCORE_PD3_FULL_CM0_wc32.

Could you please upload the fixed version of them.

And i also want to report the issue when i test the MB1303_Demo_DRP_CLI.

  1. If i want to enable the Vconn support not only define the _VCONN_SUPPORT but also _APPLI_VCONN_SUPPORT.
  2. I set the sop and sop_1 support in the usbpd_dpm_conf.h but when PE stack calls the USBPD_PHY_Init it just sets the SupportedSOP to sop.

Thanks.

BR

John.

Yohann M.
Yohann M.Best answer
ST Employee
November 12, 2019

Dear @John886​ 

Please find all the libs generated with VDM patch.

For the 2nd question, I would prefer keeping the other thread already opened by you :

=> https://community.st.com/s/question/0D50X0000BaN2XpSQK/pnucleousb002-cant-recognize-the-emarker-cable

Regards,

Yohann

Note: For your information, we posted an update of X-CUBE-USBPD under github (V3.1.0):

=> https://github.com/STMicroelectronics/x-cube-usb-pd

John886
John886Author
Associate II
November 21, 2019

Hi Yohann

Thanks for your help :)

BR

John.