Skip to main content
Associate
Apr 29, 2025 11:09 AM UTC
Question

X-CUBE STL 2.0.0 L6775W: stl_sch_main.o has FDEs which use CIEs which are not in this section.

Hello. 

I'm upgrading from version 1.0.0 to 2.0.0 of the X-CUBE STL for STMF4, but I'm struggling to resolve this warning:

Warning: L6775W: stl_sch_main.o(.debug_frame) has FDEs which use CIEs which are not in this section.

 

The warning disappears when turning of debug symbols. 

 

I'm using Arm Compiler 6.16.2 with Keil Uvision and an STM32F437. The STL version is V2.0.0 / 19-December-2022

The example projects that follow the STL package also have debug symbols enabled and produce the same warning. 

Is this an issue with how the library has been compiled, or is it possible to resolve this without disabling debug symbols or just suppressing the warning?

 

Any inputs would be greatly appreciated. 

 

 

This topic has been closed for replies.

4 replies

ST Technical Moderator
May 5, 2025 10:31 AM UTC

Hello @enlectomacto 

Please try to compare the settings of your project with those of the example projects provided with the STL package. Look for any differences in compiler settings that might be causing the issue.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate
May 5, 2025 10:41 AM UTC

Hello again, and thanks a lot for the reply. 

In the initial post I perhaps was not able to communicate clear enough the fact that the example projects provided with the STL package have the exact same issue.

The example projects give the same warning as I get in my project. 

 

Additionally, as a side note, the example projects also require a modification to the compile options to even build, which is to ensure that short wchar is disabled (ARM Compiler 6) or to set wchar size to 32 (ARM Compiler 5), since the STL lib is compiled in this way. This leads me to believe that the Keil example projects may not be particularly well maintained. 

 

 

Petr Sladecek
ST Employee
May 5, 2025 2:10 PM UTC

Hello,

pls open Release notes file at Project directory where you can read comment about the L6775W warning as well as about handling the wchar issue. This is not question of any frequent maintenance but note that whatever change of compilation parameters of the library requires recertification of the whole package what is time and cost consuming process. Anyway, the industrial STL is under NDA, so at case of trouble with this FW, please use your official ST support channel. Thank you for understanding.

Best regards,

Petr  

Associate
May 5, 2025 2:15 PM UTC

Yes I understand the difficulty of recompiling the package, I was refering to the example projects. 

But I found the comment regarding this warning in the release notes now:

  • Arm/keil: when “Debug information” is selected in Output windows of project option, a warning appears (Warning: L6775W). This warning message is only a debug information issue. It doesn’t effect the actual project at all. So it would be safe to ignore this warning

 Have a great day, thanks a lot for your help!