Skip to main content
Visitor II
Sep 20, 2024 9:50 PM UTC
Solved

X-CUBE-SMBUS 2.1.0 - Optimized builds hang when waiting on STACK_SMBUS_IsReady()

In the code examples provided with AN4502, this pattern is used often:

 

 while ( STACK_SMBUS_IsReady(pcontext) != SMBUS_SMS_READY) { }

 

But in our code, when built with the Release CMake preset, this hangs forever.

My understanding is that this is because the `StateMachine` member of the SMBus context struct (SMBUS_StackHandleTypeDef) is getting updated by the SMBUS interrupt handlers, but it isn't marked volatile:

 

 * @brief Stack state machine handling structure - the stack operation context
 */
 typedef struct
 {
 uint32_t StateMachine; /*!< Keeps track of current stack state */
 SMBUS_HandleTypeDef *Device; /*!< HAL driver handle */
 uint8_t *ARP_UDID; /*!< A UDID used in ARP */
 st_command_t *CurrentCommand; /*!< NULL, unless a command is being processed */
 st_command_t *CMD_table; /*!< Pointer to first record in the table of all supported commands */
 uint32_t CMD_tableSize; /*!< The supported commands table size */
#ifdef PMBUS13
 SMBUS_ZoneStateTypeDef TheZone; /*!< The zone structure */
#endif 
 uint16_t Byte_count; /*!< Indicates current buffer position */
 uint16_t SlaveAddress; /*!< Master remembers to which slave it is talking to */
 uint8_t OwnAddress; /*!< Device address, ARA response / Host: Address of the device that sent alert / */
 uint8_t OpMode; /*!< Operation mode (read/write) */
 uint8_t SRByte; /*!< A preset byte for use in Send byte/ Receive byte transactions */
 uint8_t Buffer[STACK_NBYTE_SIZE+2U]; /*!< The I/O buffer on which the SMBUS stack operates
 extra 2 bytes are command code and block length */
 }
 SMBUS_StackHandleTypeDef;

 

I worked around the issue by declaring our own pointer to the SMBus context, but this isn't optimal, as it marks the entire struct volatile, and causes a ton of compiler warnings to be thrown:

 

extern volatile SMBUS_StackHandleTypeDef *pcontext;

 

Saket_OmBest answer
ST Technical Moderator
May 8, 2026 3:51 PM UTC

Hello @wrigbybf 

The fix has been released in the X-CUBE-SMBUS version 2.1.1. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

2 replies

ST Technical Moderator
Sep 24, 2024 3:04 PM UTC

Hello @wrigbybf 

 

Thank you for bringing this issue to our attention.

I reported it internally to be fixed by our development team.

Internal ticket number: 191968 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Saket_OmBest answer
ST Technical Moderator
May 8, 2026 3:51 PM UTC

Hello @wrigbybf 

The fix has been released in the X-CUBE-SMBUS version 2.1.1. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om