Skip to main content
Julian1
Associate II
Feb 19, 2024 5:20 AM UTC
Question

X-CUBE-EEPROM example projects do not seem to work.

this is the same issue as previously reported in a thread that had an answer marked as a solution (it was not, in fact, a solution) 

I am looking to test X-CUBE-EEPROM on a supported eval board. (nucleo-G431RB) 

I load the relevant X-CUBE-EEPROM project into my workspace "existing projects into workspace option" 

I can see all the files and when I go to compile it "succeeds" but with 4 warnings that there are no implementations for _close_r, _lseek_r, _read_r, and _write_r

when I go to run my firmware on the target board it doesn't work (as you'd probably expect) 

When I load other target projects from the same package up in STM32 cube IDE I get the same errors when I go to build. 

I am running STM32 cube IDE 1.14.1 and AFAIK this install is auto-updating, I don't see any updates I am missing) 

the ide works fine for other projects (like the one I am actually developing, as well as an example project for a sensor I used recently to test that with an eval board before doing it in my project) but this X-CUBE-EEPROM example seems completely dead, at least if I want to use STM32 cube IDE?
. 



This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Feb 19, 2024 2:06 PM UTC

@Julian1 wrote:

I can see all the files and when I go to compile it "succeeds" but with 4 warnings that there are no implementations for _close_r, _lseek_r, _read_r, and _write_r


See: https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-13-0-problem/m-p/573904

 


@Julian1 wrote:

when I go to run my firmware on the target board it doesn't work (as you'd probably expect) 


Those are just warnings - so shouldn't necessarily stop the code from working.

You need to give more details of what, exactly, is "not working"

Use the debugger to see what's going on ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.