Skip to main content
TJack.2
Associate III
February 7, 2025
Solved

X-CUBE-DISPLAY compatibility with STM32CubeIDE

  • February 7, 2025
  • 8 replies
  • 2854 views

I am using STM32CubeIDE version 1.17.0 and trying to develop a custom board using X-CUBE-DISPLAY with a graphics display using the ST7789V controller.  This is a design update for a previous board that was using a 7-segment LCD display.  I have a preliminary version of my software running on a NUCLEO-G071RB (with external flash disabled) as a proof of concept.

When I open my .ioc file and select Manage Software Packs, it shows X-CUBE-DISPLAY as installed, versions 1.0.0 up to 3.0.0, but they are all marked with a red cross.  Hovering the mouse on 3.0.0 shows "This version of the pack is not compatible with the current version of STM32CubeIDE. It is compatible with STM32CubeIDE from 1.11.0 to 1.12.1".  Earlier versions show correspondingly early versions of the IDE.  Version 1.12.1 or earlier is no longer available on the STM32CubeIDE download page.

Does this mean support for X-CUBE-DISPLAY is discontinued, or is the message just wrong?  Is there any alternative software for entry-level graphics using SPI, that will fit in on-chip memory on a 64-pin device?  I tried using TouchGFX but it was way too bloated to be useable in this application.

Opening the .ioc file with the latest STM32CubeMX gives a similar message, however the required version of MX (6.8.1) is still available

This topic has been closed for replies.
Best answer by TJack.2
Mostly just ignored the message.  I didn't encounter any actual
incompatibilities.

I was using an ST7789V with a GT911 capacitative touchscreen.  I got MX
to generate the X-CUBE-DISPLAY graphics, deleted the memory and keypad
parts, downloaded the TC driver from GitHub, which was a bit sketchy and
needed some modifications to be compatible with the ST7789V, and reused
the USB driver (and application code) from my original 7-segment
STM32L152 project (from standard peripheral library) with a bit of
hacking to make it compatible with the STM32H503 32-bit USB access.  No
RTOS or other additional software.  All done under Linux.

Not ideal or easy, but it works.

Tim

8 replies

GaetanGodart
ST Employee
February 10, 2025

Hello @TJack.2 ,

 

TouchGFX is usable with the STM32G071RB, we even have a couple of TBS for it :

GaetanGodart_0-1739181838855.png

You will definitely be limited with such board but it is possible to use TouchGFX, we just recommend to not use any RTOS.

 

If you really want to use X-Cube, perhaps you can set it up manually (not through STM32CubeMX) : https://www.st.com/en/embedded-software/x-cube-display.html#get-software

 

"I have a preliminary version of my software running on a NUCLEO-G071RB" what do you have? I did not understand what you have done yet. SO far you have just done the project with the 7 segments screen, not with the ST7789V screen right?

 

Also, I think that you could get more help if this question was on the STM32CubeMX page instead of the TouchGFX/GUI page.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Associate III
June 17, 2025

Hello @GaetanGodart,

What about the G0B1RE? It has 144K RAM which is more than enough for RTOS and TouchGFX. I have managed to modify the G071 code for the G0B1RE; compile it, and successfully flash it. I am however, running into a set of problems during the TouchGFX initialization. 

 

Regards,

Tom

GaetanGodart
ST Employee
June 23, 2025

Hello @TS-LMG ,

 

Yes, that seems to be enough for a simple GUI.
If you require help on the TouchGFX initialization, you should create a new thread about that and provide enough information.

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
TJack.2
TJack.2Author
Associate III
February 10, 2025

My question is about STCubeIDE, not stand-alone MX.  With MX I can still download an old version that is compatible with X-CUBE-DISPLAY, but even the oldest available version of IDE claims not to be compatible, although I don't know what the issues any, if any.

With regard to my projects, yes I have made my preliminary program work on the NUCLEO with its external Flash memory.  I don't aim to use external memory on my final product as I don't intend to use images.  However if I delete the images and associated application software in the ST examples for TOUCHGFX and disable the external memory, the compilation overflows the available flash (at 170k, before addition of another 30k of my own application software). Doing the same thing with X-CUBE-DISPLAY comes in at around 30k.

My preliminary program consists of some text and basic shapes on the screen as a proof-of-concept, which I have successfully tested on NUCLEO-G071 with both TOUCHGFX and X-CUBE-DISPLAY.

My target processor is STM32H503 as my application needs USB-Device.  That gives me a Flash budget of 128k. I have no need of any 3rd party RTOS.

This is background information to explain my position.  I reiterate that my question is whether or not ST intend to produce a version of X-CUBE-DISPLAY that is officially compatible with the latest version of STCubeIDE, as the current version isn't.

 

GaetanGodart
ST Employee
June 23, 2025

Hello @TJack.2 ,

 

Yes I understand, I was just answering to enquiries about size and compatibility of TouchGFX and STM32GG071RB.
I was hoping someone else would answer for the other question.

 

I seem to not fully understand the issue though. Since you are talking about enabling X-Cube-XXX, I assume you were on the STM32CubeMX that is embedded in the STM32CubeIDE software, so to me this is an STM32CubeMX question even if you are opening STM32CubeIDE. Perhaps we could clarify this.
For instance, here is a brand new STM32G071RB project created using STM32CubeIDE, but as I create the project, it embeds STM32CubeMX:

GaetanGodart_0-1750667134376.png

In this project, I am not able to enable X-CUBE-DISPLAY, but if I create a STM32G071RB project from STM32CubeMX, it is also not compatible with my version but it is compatible with older versions of STM32CubeMX that are available for download on the official webpage.

 

Also, have screenshots and maybe the project file could help us.

 

"whether or not ST intend to produce a version of X-CUBE-DISPLAY that is officially compatible with the latest version of STCubeIDE, as the current version isn't"
I don't think so, TouchGFX is the preferred graphical interface right now.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
TJack.2
TJack.2Author
Associate III
June 27, 2025
I can't log in to ST community any more to reply to this.  It sends me
to a Microsoft account which say as this.

FWIW my original query was about the following error message from cube
1.17.0.

However the project worked (after a lot of hacking) despite the apparent
error.

Tim Jackson