Skip to main content
Ronan Gaillard
Associate
March 22, 2018
Question

WRP bits not working ?

Posted on March 22, 2018 at 11:06

Hi,

I am working with the STM32f407 : I have a bootloader in the first flash sector (ie. @ 0x0800 0000), and my main program in the following sectors (ie. @ 0x0800 4000). I want to protect my bootloader against unwanted writes, so I used the WRP bits to protect it.

What I've done is write 0xFFFE (ie. Sector 0 with write protection enable) to the 0x1FFF C008 Option Bytes. By reading it back I'm sure that it has been well written. (I'm writing the Option Bytes by DFU using dfu-utils).

After reset I am able to write to sector 0 using either DFU or ST-LINK, which I should not be allowed to.

Am I missing something ?

Best,

Ronan

#wrp #dfu #option-bytes #stm32f407
This topic has been closed for replies.

6 replies

waclawek.jan
Super User
March 22, 2018
Posted on March 22, 2018 at 13:06

Can you read out and check the option bytes using ST-Link?

JW

Ronan Gaillard
Associate
March 22, 2018
Posted on March 22, 2018 at 14:55

Hi,

I am able to read bytes by using 

st-flash read tmp.bin 0x1fffc008 1

Which result in a file containing 0x00f0ff0f

But I am not able to write using 

st-flash write tmp.bin 0x1fffc008

The result is : Unknown memory region

Also in the finished product the only access to the stm32 will be by USB, so I would like to manipulate WRP bytes by DFU.

Thanks for your time !

waclawek.jan
Super User
March 22, 2018
Posted on March 22, 2018 at 16:01

What is st-flash?

If 0x00f0ff0f is content of memory on 0x1fffc008, then it's clearly not set to 0xFFFE, is it?

Can you try the ST-Link Utility to read out or set  the option bytes?

JW