Skip to main content
BLász.1
Visitor II
May 14, 2023 7:16 PM UTC
Question

Windows doesn't recognise my Nucleo as a sound device

Hi everyone!

Sorry if it's a newbie question, I just started learning this. I used USB_DEVICE middleware to make the code for the Audio Device Class. Even though I increased the heap to 2800h Windows doesn't recognise it as a sound device. I'm using the Nucleo F446RE. Am I missing drivers? Thanks in advance.

This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
Jun 7, 2023 8:33 AM UTC

Hello @Bálint László​ and welcome to the Community :) ,

Which Windows system are you using?

If you use Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x, it should installed the STM32 Virtual COM Port Driver must be installed in this case.

Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in. So, no driver is required for W10.

Also, try to use static allocation, as recommended in this FAQ.

I hope this help you!

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Piranha
Principal III
Jun 7, 2023 10:44 PM UTC

The autor is talking about audio device, not CDC (virtual COM port). Next time try actually reading the topic...