Skip to main content
PWind.1
Associate
September 3, 2020
Question

Windows 10 CDC issues

  • September 3, 2020
  • 0 replies
  • 417 views

Following on from previous thread I can now get the CDC to be sen by Windows, but unless the clock source is set to PLL and running at 120MHz, opening and closing ports on the Windows machine causes programs to hang.

It all runs fine if the port communicates under Linux.

Does anyone have any suggestions for getting the CDC to run under Windows at lower clock speeds?

Thanks

This topic has been closed for replies.