Skip to main content
FCamp.1
Associate III
Jun 1, 2020 8:17 PM UTC
Solved

Why TIMER takes time to start up?

Hi,

I have a F439ZI where i have set a simple timer (TIM10) to raise the the HAL_TIM_PeriodElapsedCallback every 1 millisecond.

The Bus APB2 for timers runs at 168 MHz so i set in the configuration 168 in the prescaler (result is 1Mhz) and the i set 1000 in the counter period.

In fact he callback is fired every millisecond as expected. Problem is that it takes around 6 seconds to fire for the first time.

Any idea why?

Thanks a in advance,

Filo

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jun 1, 2020 8:40 PM UTC

> it takes around 6 seconds to fire for the first time.

How do you know?

Is there any other software there, blocking the interrupts - or delays setting up the timer - for about 6 seconds?

JW

11 replies

waclawek.jan
waclawek.janBest answer
Super User
Jun 1, 2020 8:40 PM UTC

> it takes around 6 seconds to fire for the first time.

How do you know?

Is there any other software there, blocking the interrupts - or delays setting up the timer - for about 6 seconds?

JW

berendi
Principal
Jun 2, 2020 11:15 AM UTC

Do you measure the 6 seconds from starting the timer, or from powering up/resetting the MCU?

I've played a bit with HAL recently and found that a certain initialization function takes exactly 3 seconds before it silently fails.

waclawek.jan
Super User
Jun 2, 2020 11:30 AM UTC

Silently? Not even returning some error code?

There are peripherals which legitimately take seconds to start up, e.g. a well designed LSE oscillator.

JW

berendi
Principal
Jun 4, 2020 6:24 AM UTC

Yes, CubeMX initialization code silently ignores errors, the only indication is that it takes an an integer multiple of a second longer than it should.

RTC initialization gets confused when the RTC is already running. I was under the impression that the point of having a RTC is to keep it running, but apparently my view is not shared by the CubeMX developers.

HAL functions actually return HAL_ERROR. Very helpful.

MX_RTC_Init() is declared void, but it at least calls Error_Handler() three times. Which has no parameters, so again very helpful. What am I supposed to do, count how many times Error_Handler() was called to determine the nature of the error?

This stuff should be banned. It is harmful. Not just considered harmful, but matter-of-fact harmful.

FCamp.1
FCamp.1Author
Associate III
Jun 2, 2020 11:34 AM UTC

Hello,

yes i mean 6 second from the powerup of the device.

Anyway I have fixed, waclawek.jan was right.

There was a ETH service set by CUBEMX by default that was taking time to initialize. The initialization was set in the code before then the TIM start instruction.

Once disabled this service everything went fine.

Thanks a lot to both,

Filo