Skip to main content
Oct 23, 2022 11:56 AM UTC
Question

Why MSC_REQUEST_SENSE results in No error when there is error in the sense key ?

I have connected a turned off android phone to the stm32 USB port.

Device gets enumerated as a msc device.

Enumeration output

USB Device Connected

USB Device Reset Completed

PID: 2eb7h

VID: 22b8h

Address (#1) assigned.

Manufacturer : motorola

Product : moto g(9) play

Serial Number : ZY3282Q2V5

Enumeration done.

This device has only 1 configuration.

Default configuration set.

Switching to Interface (#0)

Class : 8h

SubClass : 6h

Protocol : 50h

MSC class started.

Number of supported LUN: 1

LUN #0:

Inquiry Vendor : Linux

Inquiry Product : File-Stor Gadget

Inquiry Version : 0419

Sense Key : 2

Additional Sense Code : 3a

Additional Sense Code Qualifier: 0

Sense Key : 2

Additional Sense Code : 3a

Additional Sense Code Qualifier: 0

ERROR: USB Disk is not ready!

device gets enumerated as a MSC Device

Why the device is not ready and there is no checking of the readiness of the USB MSC in activating this class in the line of 528 of usbh_msc.c ?

phost->pUser(phost, HOST_USER_CLASS_ACTIVE);

#USB #STM32F7​ #[STM32 MCUs]​ 

This topic has been closed for replies.