Skip to main content
Associate III
Feb 9, 2026 12:38 PM UTC
Solved

Why is AXI RAM and RIF necessary when using DCMIPP?

Hello, i just wanna take a snapshot by STM32N6570-DK with IMX335. I am using SnapshotDecimation as my reference. after reviewing the code. i wonder why AXI RAM3/4 and RIF are necessary for this project i saw it in 'HAL_DCMIPP_MspInit' function, but i didnt found anything about AXI RAM in other parts of the code.

anyone can explain why does axiram necessary for this project?

void HAL_DCMIPP_MspInit(DCMIPP_HandleTypeDef* hdcmipp)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 RAMCFG_HandleTypeDef hramcfg = {0};
 RIMC_MasterConfig_t RIMC_master = {0};
 if(hdcmipp->Instance==DCMIPP)
 {
 /* USER CODE BEGIN DCMIPP_MspInit 0 */
 /*** Enable peripheral clock ***/
 /* Enable DCMIPP clock */
 __HAL_RCC_DCMIPP_CLK_ENABLE();

 __HAL_RCC_DCMIPP_FORCE_RESET();
 __HAL_RCC_DCMIPP_RELEASE_RESET();

 /*** Configure the NVIC for DCMIPP ***/
 /* NVIC configuration for DCMIPP transfer complete interrupt */
 HAL_NVIC_SetPriority(DCMIPP_IRQn, 0x07, 0);
 HAL_NVIC_EnableIRQ(DCMIPP_IRQn);

 /*** Enable peripheral clock ***/
 /* Enable CSI clock */
 __HAL_RCC_CSI_CLK_ENABLE();

 __HAL_RCC_CSI_FORCE_RESET();
 __HAL_RCC_CSI_RELEASE_RESET();

 /*** Configure the NVIC for CSI ***/
 /* NVIC configuration for CSI transfer complete interrupt */
 HAL_NVIC_SetPriority(CSI_IRQn, 0x07, 0);
 HAL_NVIC_EnableIRQ(CSI_IRQn);

 /* USER CODE END DCMIPP_MspInit 0 */
 /* USER CODE BEGIN DCMIPP_MspInit 1 */

 /* DCMIPP Clock Config */
 /* DCMIPP clock configuration */
 /* Typical PCLK is 333 MHz so the PLL1 is configured to provide this clock */
 /* Configure DCMIPP clock to IC17 with PLL1 */
 /* PLL1_VCO Input = HSI_VALUE/PLLM = 64 Mhz / 4 = 16 */
 /* PLL1_VCO Output = PLL3_VCO Input * PLLN = 16 Mhz * 75 = 1200 */
 /* PLLLCDCLK = PLL3_VCO Output/(PLLP1 * PLLP2) = 1200/4 = 300Mhz */
 /* DCMIPP clock frequency = PLLLCDCLK = 300 Mhz */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DCMIPP;
 PeriphClkInitStruct.DcmippClockSelection = RCC_DCMIPPCLKSOURCE_IC17;
 PeriphClkInitStruct.ICSelection[RCC_IC17].ClockSelection = RCC_ICCLKSOURCE_PLL1;
 PeriphClkInitStruct.ICSelection[RCC_IC17].ClockDivider = 4;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_CSI;
 PeriphClkInitStruct.ICSelection[RCC_IC18].ClockSelection = RCC_ICCLKSOURCE_PLL1;
 PeriphClkInitStruct.ICSelection[RCC_IC18].ClockDivider = 60;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* IMX335 Sensor HW Reset */
 /* Enable GPIO clocks */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 GPIO_InitTypeDef gpio_init_structure = {0};

 /* Initialize camera NRST pin */
 gpio_init_structure.Pin = GPIO_PIN_8;
 gpio_init_structure.Pull = GPIO_NOPULL;
 gpio_init_structure.Mode = GPIO_MODE_OUTPUT_PP;
 gpio_init_structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init(GPIOC, &gpio_init_structure);

 /* Initialize camera EN pin */
 gpio_init_structure.Pin = GPIO_PIN_2;
 gpio_init_structure.Pull = GPIO_NOPULL;
 gpio_init_structure.Mode = GPIO_MODE_OUTPUT_PP;
 gpio_init_structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init(GPIOD, &gpio_init_structure);

 /* Camera sensor Power-On sequence */
 /* Assert the camera Enable and NRST pins */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_8, GPIO_PIN_SET);
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_RESET);
 HAL_Delay(200); /* NRST and Enable signals asserted during 200ms */

 /* De-assert the camera STANDBY pin (active high) */
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_SET);
 HAL_Delay(3); /* NRST de-asserted during 3ms */

 /* SRAM3 and SRAM4 memories clock enable */
 LL_MEM_EnableClock(LL_MEM_AXISRAM3);
 LL_MEM_EnableClock(LL_MEM_AXISRAM4);

 /* Power On AXSRAM3 and AXISRAM4 */
 hramcfg.Instance = RAMCFG_SRAM3_AXI;
 HAL_RAMCFG_EnableAXISRAM(&hramcfg);

 hramcfg.Instance = RAMCFG_SRAM4_AXI;
 HAL_RAMCFG_EnableAXISRAM(&hramcfg);

 __HAL_RCC_RIFSC_CLK_ENABLE();

 RIMC_master.MasterCID = RIF_CID_1;
 RIMC_master.SecPriv = RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV;

 HAL_RIF_RIMC_ConfigMasterAttributes(RIF_MASTER_INDEX_DCMIPP, &RIMC_master);
 HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_DCMIPP , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV);
 /* USER CODE END DCMIPP_MspInit 1 */
 }

}

 

Ch_JEBest answer
ST Employee
Feb 13, 2026 2:54 PM UTC

Hello ,

the AXI SRAM3 and 4 are used as camera frame buffer #define BUFFER_ADDRESS 0x34200000 

Ch_JE_0-1770993428659.png

For the RIF part: DCMIPP is a bus master and therefore needs its RIF master and slave attributes to be configured; otherwise, its transfers to RAM will be blocked. Configure the master attributes to authorize DCMIPP’s memory accesses, and configure the slave attributes to authorize CPU access to DCMIPP registers.

Best Regards,

1 reply

Ch_JEBest answer
ST Employee
Feb 13, 2026 2:54 PM UTC

Hello ,

the AXI SRAM3 and 4 are used as camera frame buffer #define BUFFER_ADDRESS 0x34200000 

Ch_JE_0-1770993428659.png

For the RIF part: DCMIPP is a bus master and therefore needs its RIF master and slave attributes to be configured; otherwise, its transfers to RAM will be blocked. Configure the master attributes to authorize DCMIPP’s memory accesses, and configure the slave attributes to authorize CPU access to DCMIPP registers.

Best Regards,