Skip to main content
CDyer.1
Associate III
Apr 3, 2025 9:23 AM UTC
Question

Why is a fresh FreeRTOS project using all my RAM? How can I determine the root cause?

Hi, see above. I am using a custom G030F6 breakout board with the intent to install FreeRTOS and use this small device as a learning exercise as I usually use larger MCUs and super loops. My first hurdle is my RAM usage with a blank, generated projected. I get the following error when I configure FreeRTOS using STM32CubeIDE (I also get the same error if i import freertos manually and use the same memory allocations) and then compile a brand new project:

section `._user_heap_stack' will not fit in region `RAM'

I understand this to mean that my memory allocations are too large to fit within the available RAM. My chosen device has RAM of 8KB. My config is as follows:

 

#ifndef FREERTOS_CONFIG_H
#define FREERTOS_CONFIG_H

/*-----------------------------------------------------------
 * Application specific definitions.
 *
 * These definitions should be adjusted for your particular hardware and
 * application requirements.
 *
 * These parameters and more are described within the 'configuration' section of the
 * FreeRTOS API documentation available on the FreeRTOS.org web site.
 *
 * See http://www.freertos.org/a00110.html
 *----------------------------------------------------------*/

/* USER CODE BEGIN Includes */
/* Section where include file can be added */
/* USER CODE END Includes */

/* Ensure definitions are only used by the compiler, and not by the assembler. */
#if defined(__ICCARM__) || defined(__CC_ARM) || defined(__GNUC__)
 #include <stdint.h>
 extern uint32_t SystemCoreClock;
#endif
#ifndef CMSIS_device_header
#define CMSIS_device_header "stm32g0xx.h"
#endif /* CMSIS_device_header */

#define configENABLE_FPU 0
#define configENABLE_MPU 0

#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 1
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 56 )
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)3072)
#define configMAX_TASK_NAME_LEN ( 16 )
#define configUSE_TRACE_FACILITY 1
#define configUSE_16_BIT_TICKS 0
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 8
#define configUSE_RECURSIVE_MUTEXES 1
#define configUSE_COUNTING_SEMAPHORES 1
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 0
/* USER CODE BEGIN MESSAGE_BUFFER_LENGTH_TYPE */
/* Defaults to size_t for backward compatibility, but can be changed
 if lengths will always be less than the number of bytes in a size_t. */
#define configMESSAGE_BUFFER_LENGTH_TYPE size_t
/* USER CODE END MESSAGE_BUFFER_LENGTH_TYPE */

/* Co-routine definitions. */
#define configUSE_CO_ROUTINES 0
#define configMAX_CO_ROUTINE_PRIORITIES ( 2 )

/* Software timer definitions. */
#define configUSE_TIMERS 1
#define configTIMER_TASK_PRIORITY ( 2 )
#define configTIMER_QUEUE_LENGTH 10
#define configTIMER_TASK_STACK_DEPTH 256

/* The following flag must be enabled only when using newlib */
#define configUSE_NEWLIB_REENTRANT 1

/* CMSIS-RTOS V2 flags */
#define configUSE_OS2_THREAD_SUSPEND_RESUME 1
#define configUSE_OS2_THREAD_ENUMERATE 1
#define configUSE_OS2_EVENTFLAGS_FROM_ISR 1
#define configUSE_OS2_THREAD_FLAGS 1
#define configUSE_OS2_TIMER 1
#define configUSE_OS2_MUTEX 1

/* Set the following definitions to 1 to include the API function, or zero
to exclude the API function. */
#define INCLUDE_vTaskPrioritySet 1
#define INCLUDE_uxTaskPriorityGet 1
#define INCLUDE_vTaskDelete 1
#define INCLUDE_vTaskCleanUpResources 0
#define INCLUDE_vTaskSuspend 1
#define INCLUDE_vTaskDelayUntil 1
#define INCLUDE_vTaskDelay 1
#define INCLUDE_xTaskGetSchedulerState 1
#define INCLUDE_xTimerPendFunctionCall 1
#define INCLUDE_xQueueGetMutexHolder 1
#define INCLUDE_uxTaskGetStackHighWaterMark 1
#define INCLUDE_xTaskGetCurrentTaskHandle 1
#define INCLUDE_eTaskGetState 1

/*
 * The CMSIS-RTOS V2 FreeRTOS wrapper is dependent on the heap implementation used
 * by the application thus the correct define need to be enabled below
 */
#define USE_FreeRTOS_HEAP_4

/* Normal assert() semantics without relying on the provision of an assert.h
header file. */
/* USER CODE BEGIN 1 */
#define configASSERT( x ) if ((x) == 0) {taskDISABLE_INTERRUPTS(); for( ;; );}
/* USER CODE END 1 */

/* Definitions that map the FreeRTOS port interrupt handlers to their CMSIS
standard names. */
#define vPortSVCHandler SVC_Handler
#define xPortPendSVHandler PendSV_Handler

/* IMPORTANT: After 10.3.1 update, Systick_Handler comes from NVIC (if SYS timebase = systick), otherwise from cmsis_os2.c */

#define USE_CUSTOM_SYSTICK_HANDLER_IMPLEMENTATION 0

/* USER CODE BEGIN Defines */
/* Section where parameter definitions can be added (for instance, to override default ones in FreeRTOS.h) */
/* USER CODE END Defines */

#endif /* FREERTOS_CONFIG_H */

 

If my heap is 3KB and stack is configured to be 256 Bytes, where is the other 5KB being used?

thanks in advance.

 

Edit: reducing heap size to 2KB resulted in a successful compilation, but I still want to know what the original cause is. Where is my RAM being used. Fully compiled blank project attached. Thanks all.

This topic has been closed for replies.

6 replies

unsigned_char_array
Lead III
Apr 3, 2025 9:46 AM UTC

Can you upload your linker file?
Can you upload your map file (or screenshot of memory analyzer in STM32CubeIDE)? (if not possible without a completed build, try setting the stack and heap sizes very low so it builds)
My suspicion is that non-RTOS stack and non-RTOS heap are too big. Non-RTOS stack only needs to be big enough to setup the RTOS, then every task will use its own stack. You might not need heap at all.
8 kiB is very low for an RTOS. You might consider something else such as stackless microthreads/co-routines.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Andrew Neil
Super User
Apr 3, 2025 9:47 AM UTC

@CDyer.1 wrote:

 I am using a custom G030F6 breakout board with the intent to install FreeRTOS and use this small device as a learning exercise as I usually use larger MCUs .


That seems a bizarre approach?

Surely, larger processors are going to be more appropriate to an RTOS - any RTOS ?!

For an RTOS learning exercise, you don't want to start by battling resource constraints.

 

In fact, for learning FreeRTOS there's a simulator - so you don't even need an embedded target at all:

https://freertos.org/Documentation/02-Kernel/03-Supported-devices/04-Demos/03-Emulation-and-simulation/01-Emulation-and-simulation

 

But, for any project, the way to see the memory usage is to look at the Map file...

Plus, in CubeIDE, there's the Build Analyser

 

AndrewNeil_0-1743673650750.png

https://www.st.com/resource/en/user_manual/dm00629856.pdf#page=76

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
CDyer.1
CDyer.1Author
Associate III
Apr 3, 2025 10:07 AM UTC

Thanks for the link to the simulator, I'm sure that may come in handy in the future. In response to your initial point, it is outside the scope of the question but there is a good reason for it. I just want to solve the question posted. Regarding the build analyser, for some reason despite having both a .elf and .map (now I've compiled and reduced the heap size) it's still blank. 

unsigned_char_array
Lead III
Apr 3, 2025 11:34 AM UTC

@CDyer.1 wrote:

Regarding the build analyser, for some reason despite having both a .elf and .map (now I've compiled and reduced the heap size) it's still blank. 


You can refresh the build analyzer:

unsigned_char_array_0-1743679726052.png

 

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."