Skip to main content
Prajnyajit
Associate III
Sep 28, 2021 11:15 AM UTC
Question

Why I'm unable to use UART to upload a program to NUCLEO L476?

I'm using Nucleo-L476RG as MCU. I am trying to upload a program to it using UART.

  1. I have tried connecting the BOOT0 with VDD.
  2. Rx/D0 with Rx of FTDI (USB to TTL cable).
  3. Tx/D1 with Tx of FTDI.
  4. The ground of FTDI with Ground of Nucleo.

I am using STM32 Flasher to upload the program but am unable to do so. I have tried another way to put MCU into bootloader mode which is pressing the USER button still no result. Why?

This topic has been closed for replies.

4 replies

Uwe Bonnes
Chief
Sep 28, 2021 11:47 AM UTC

Did you try cross connection?

Prajnyajit
Associate III
Sep 28, 2021 11:50 AM UTC

Yes! Already done. No improvement.

TDK
Sep 28, 2021 12:57 PM UTC

> Rx/D0 with Rx of FTDI (USB to TTL cable).

> Tx/D1 with Tx of FTDI.

RX and TX must be crossed. In other words, the TX signal transmitted by the adapter must be connected to the UART_RX pin on the MCU.

Also note that the onboard ST-Link may be holding the chip in reset. Upgrade firmware or otherwise verify NRST is high.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Prajnyajit
Associate III
Sep 28, 2021 2:34 PM UTC

checked it all. I think it wont be possible because USB is already connected so first it needs to be desoldered then only serial/UART can be possible.