Skip to main content
BParh.1
Senior III
Apr 28, 2021 4:47 AM UTC
Solved

Why I can't find the source code for the demo in the development board?

So I bought STM32F769 Discovery Board for prototyping. In BoardOverview doc states the demonstration source code could be found in www.st.com/stm32f7-discovery

But I could not find it there, it only provide the compiled binary which is not much of a help. I would like to use the source code as reference.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 28, 2021 5:45 AM UTC

Yes, the ZIP file contains the compiled demo for the 32F769IDISCOVERY, but also the required media files (audio, video, pictures).

You can find the source code in the repository, either on your computer as part of the downloaded firmware, or on Github.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 28, 2021 5:45 AM UTC

Yes, the ZIP file contains the compiled demo for the 32F769IDISCOVERY, but also the required media files (audio, video, pictures).

You can find the source code in the repository, either on your computer as part of the downloaded firmware, or on Github.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BParh.1
BParh.1Author
Senior III
Apr 28, 2021 7:02 AM UTC

Thank you @Peter BENSCH​ , that was I looking for but I could not find any of the STM32CubeMX (.ioc) file in the Github. Sometimes I want to see how the hardware setup. Was it only meant to open using IAR or Keil IDE?

Peter BENSCH
ST Technical Moderator
Apr 28, 2021 7:33 AM UTC

Well, the demo was prepared a few years ago and IOC files weren't always attached back then.

In the repository you will find the project folders for the commercial IDE from IAR and Keil, as well as one for SW4STM32 (aka AC6, GNU GCC based), which you can easily import into STM32CubeIDE.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Apr 28, 2021 5:51 AM UTC

> as part of the downloaded firmware

By "firmware" Peter meant the CubeF7 "library", which you can download standalone as a package from ST's website, or you can access its current version through github as Peter linked above; but what Peter assumed is, that you've downloaded and run CubeIDE (or CubeMX) and then it gets downloaded as part of the "magic" allowing you to generate code by clicking.

JW