Skip to main content
BNiro.1
Visitor II
Jun 30, 2022 8:08 PM UTC
Question

Why does MX_LWIP_Init() and the LwIP stack only works on DefaultTask?

Hello there!

I am working on a STM32F407 project with an Ethernet port through which I am setting up a TCP client with LwIP and also managing a couple of other tasks with FreeRTOS.

The code generator writes the MX_LWIP_Init() function in the defaultTask, and if I run the entire client in this task, it works great (I'm using the netconn functions to connect and send/receive data).

But my biggest question is what is so special about this task? because when I try to run the client in other tasks it doesn't work at all. Even to the point where if I want to run MX_LWIP_Init() in another task, it throws the hardfault handler (I'm disabling all other tasks during the test so they don't interfere)

I find this quite annoying because I can't use the LwIP features in any other task besides the default task.

This topic has been closed for replies.