Skip to main content
SGian.1
Associate III
Jan 14, 2026 7:33 PM UTC
Solved

Why does HAL_I2C_Mem_Read_IT return OK for a wrong address?

Hi there !

I use thi function and work perfectly . But if i try to read the HAL_StatusTypeDef   i don't understand why return HAL_OK even if i wrote a wrong address why ???? 

if i use void HAL_I2C_ErrorCallback(I2C_HandleTypeDef *hi2c)    this work with i wrote a wrong address 

please some one can tell me why ?

 

Thank you 

Sergio

Andrew Neil
Andrew NeilBest answer
Super User
Jan 15, 2026 9:16 AM UTC

@SGian.1 wrote:

 i don't understand why return HAL_OK even if i wrote a wrong address


What do you mean by "wrong address" here - I2C Slave address, or some other (memory) address?

If it's the I2C Slave address, then the code has no way to tell in advance what slave addresses are present in your external hardware - so it can't tell in advance if the address is "valid" or not.

 

PS:

You can use HAL_I2C_IsDeviceReady() to check if a particular Slave address device is present & responding on the bus.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

5 replies

Chris21
Associate II
Jan 14, 2026 9:35 PM UTC


You can look at the HAL source code to see what error conditions the function checks for.

Null pointer, 0 length -> HAL_ERROR

I2C in use already -> HAL_BUSY

Other erroneous possibilities are not checked for.

There are some HAL functions that always return HAL_OK.

if (hi2c->State == HAL_I2C_STATE_READY)
{
 if ((pData == NULL) || (Size == 0U))
 {
 hi2c->ErrorCode = HAL_I2C_ERROR_INVALID_PARAM;
 return HAL_ERROR;
 }

 if (__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BUSY) == SET)
 {
 return HAL_BUSY;
 }

Edited to apply source code formatting - please see How to insert source code for future reference.

.
Pavel A.
Jan 15, 2026 5:24 AM UTC

Because this function is asynchronous. When it returns, the target device has not responded (or not) yet. So the error callback is the only way to know the outcome.

 

 

 

Andrew Neil
Andrew NeilBest answer
Super User
Jan 15, 2026 9:16 AM UTC

@SGian.1 wrote:

 i don't understand why return HAL_OK even if i wrote a wrong address


What do you mean by "wrong address" here - I2C Slave address, or some other (memory) address?

If it's the I2C Slave address, then the code has no way to tell in advance what slave addresses are present in your external hardware - so it can't tell in advance if the address is "valid" or not.

 

PS:

You can use HAL_I2C_IsDeviceReady() to check if a particular Slave address device is present & responding on the bus.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
SGian.1
SGian.1Author
Associate III
Jan 15, 2026 10:00 AM UTC

I mean i try to send another address just check if i receive HAL_ERROR or somethingh else. 

Thank you all you guys for the help

Andrew Neil
Super User
Jan 15, 2026 10:31 AM UTC

So as @Pavel A. and I both said, the software cannot know in advance whether an address is or is not active on the external bus:  it can only tell that by receiving the ACK or NACK - and that only becomes available in the callback.

If you want to know immediately, you have to use the synchronous (blocking) API.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.